Part Number: MSP430FR2110 Hi Experts,
Good day. We have this query from Cx:
MSP430FR2110 - Is it possible to access PORT input bits byte-wise?
Thank you!
Regards, Archie A.
Part Number: MSP430FR2110
We now have the MSP430FR2110 Installed and are able to use BSL to get a full set of transactions (see attached Saleae capture) We are not however actually seeing if any of the code is running after we do a reset. We would expect…
Part Number: MSP430FR2110 I am using Code Composer Studio 10.1.00010. When i use the MSP430 Hex Utility, I have it set to give me a TI TXT file. The File contains everything I need except the reset vector value. I have seen in many TI TXT example files…
Part Number: MSP430FR2110 Hello team,
My customer are using MSP430FR2110, they are just wondering what is the IO voltage level of BSL (Bootloader) for this device ? Whether it is same for BSL through UART and BSL through SBW ?
Regards,
Renan
Part Number: MSP430FR2110 Hi Team,
Can you please check and advise with following request:
"
i want to use TB0.1(P2.0) pin as capture input. Also you know there is just one timer B0 in msp430fr2110. But TB0.1 pin is controled by CCI1A and TB1 module…
Part Number: MSP430FR2110 Hi Team,
I have following request, can you please check and advise:
"
I am having the problem in the picture below. Although the 1 byte register is 0 in the condition, the condition does not occur. Can you help with this…
Part Number: MSP430FR2110 This error was appeared on working. I did not understand what happened. The program was crash during work. You can see error screenshots and code at the attach.
Could you please help me about this problem urgently?
Thanks and…
Part Number: MSP430FR2110 Hi team,
My customers are looking for a cost-effective MCU for below application:
1 channel comparator
generate 6-bit 500kHz PWM (so the resolution should be: 1/500000/(2^6)=31.25ns)
Can they use MSP430FR2110?
If cannot, could…
Part Number: MSP430FR2110 Hello everyone, Use MSP430FR2110. MCLK is 16MHz. The required specification requires a startup time of 40 ms or less. I would like some data on the convergence characteristics of FLL lock.
Thank you in advance.
Best regards,
k.…