Part Number: MSP430FR2433 Other Parts Discussed in Thread: UNIFLASH Hi,
I'm working with the built-in bootloader which erases the information FRAM section when given a bad password. Is there a way to protect this memory section from getting erased…
Part Number: MSP430FR2433 HI TI,
I tried to debug the code on my customized MSP430FR2433IRGER MCU using MSP430FR2433 Launchpad through EZ-FET probe.
but Iam getting error "MSP430: Error connecting to the target: Unknown device." Can you suggest some ideas…
Part Number: MSP430FR2433
Hi,
Which library file and header do I use for the MSP430FR24433 with CCS 12.5.0? I installed it but it's not an option in CCS products.
Regards,
-Mike
Part Number: MSP430FR2433 Hi Team,
customer is using MSP430FR2433 and is interested M0 based alternative.
He is looking for a MCU that has the same performance at a lower cost or higher performance at the same cost.
What would be some options here?
BR…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: MSP-EXP430FR2433 Hi,
I'm using CCS to run and debug an MSP430FR2433 using the MSP-EXP430FR2433. I then remove jumpers to RXD/TXD/SBWTDIO/SBWTCK and connect a BSL interface.
I then invoke the…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: MSP430WARE Hi There,
I am working with MSP430FR2433 using msp430ware Version 3.80.14.01, curious about how I2C works,
so checked in Oscilloscope for pin P1.3, P1.2 in debug mode by resuming, both…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: UNIFLASH Hi,
How do I use the BSL-Scripter on Windows 10 to do a simple TX_BSL_VERSION so I can see the BSL invoke sequence on TEST/RST and capture a command/response?
Regards,
-Mike
Part Number: MSP430FR2433
Hi Champ,
I am asking for my customer.
It is a FA returned case, and the device was MP'ed for few years already. (Failure rate: 153/32000 pcs)
The device was all programmed successfully, then mounted it to the daughter card…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: MSP430WARE
I've created a new CCS project (v12.5) and have installed the MSP430Ware kit via the resource explorer. Then, following the instructions documented in MSP430FR2xx_4xx_DriverLib_Users_Guide…