Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP-FET , MSP430FR5962 , MSP430FR5964 , MSP430FR5994 , MSP430FR5992 , When I have the MSP-FET connected to the MSP430, the chip responds properly to low reset pulse. The chip resets and starts execution…
Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP-FET I have a new MSP430 board that is not booting. This was a working design with the previous board. As far as I can tell it has power and I am able to program it with the MSP-FET. That is…
Part Number: MSP430FR59941 Hi Team,
Now, I am trying to develop an application need to preserve the system status into FRAM when the power is down.
Could you provide me with the layout of FRAM, RAM, registers, caches?
If possible, would you give me some…
Part Number: MSP430FR59941
Hi Team,
Our customer uses the MSP430 chip as SPI master to transfer characters to nrf52840 chips (slaves), but the received characters always include a garbled character in the most front, it is like a triangle shape. How…
Part Number: MSP430FR59941 When I try to connect devices by SPI interfaces, I am not sure what's the meaning of the UCA0STE pin? Should it connect to the slave device? How to connect?
Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP430FR5994 , MSP-EXP430FR5994 ,
Hi Experts,
Good day. I would like to confirm if the development board MSP-EXP430FR5994 (for MSP430FR5994) is also compatible for MSP430FR59941.
Does putting MSP430FR59941…
Part Number: MSP430FR59941 Other Parts Discussed in Thread: UNIFLASH Hi there,
I am currently working on creating a script which will be used to flash an MSP430FR5994IPNR and then conduct hardware/software tests on the circuit board on which it is hosted…
Part Number: MSP430FR59941 Hi Sir
When using I2C BSL, there will be occasional lock-up and no response. Re-send BSL to enter sequence can not be released, you need to re-power on VCC,
Because the system has a backup power supply, in fact VCC always exists…
Part Number: MSP430FR59941
Hello everyone,
I am trying to load a custom library on the MSP430. Among many files, a common error that I am observing is this - #2633 - Modifiers not allowed in printf_support=minimal mode.
An example of the line that throws…