Part Number: MSP430FR6820 I need clarification on the operation of the BOR reset circuitry and trigger thresholds in the MSP430FR6820.
Table 5-1 in section 5.13.1 Power Supply Sequencing in the datasheet states Min and Max values for V_VCC_BOR- and V_VCC_BOR…
Part Number: MSP430FR6820 MSP430 Friends & Family,
Our customer is asking the following of the FR6820 BOR detect function:
From the TI datasheet, if RST pin voltage is lower than 1.66V and the duration is longer than 2usec, we believe it would trigger…
Part Number: MSP430FR6820 MSP430 Friends & Family,
Our customer is in need of 3D models of MSP430FR6820IPMR and MSP430FR6820IRGCR.
If available, please provide?
TY, CY
Part Number: MSP430FR6820
Tool/software: TI C/C++ Compiler
Hello team,
we are working on code optimization. Currently using -O0 level of optimization (page 55, SLAU132R), but since we are limited on memory, we may need to change to -O1 level.
That level…
Part Number: MSP430FR6820 Other Parts Discussed in Thread: MSP430FR2311 Tool/software: Code Composer Studio I can create and use a FRAM variable. It is not difficult. But I need to
create a variable (an array of bytes about 1kB) with a constant address…
Part Number: MSP430FR6820 Hi Team,
1) Can you advise what is the lower limit for RAM voltage - i.e. what voltage causes that RAM is lost?
2) If we have SVSHE=1, device should reset at 1.75V-1.85V and all pins would be in high impedance, is it right?
…
Part Number: MSP430FR6820 Other Parts Discussed in Thread: MSP430FR6822 , Tool/software: Code Composer Studio Hello,
we need to get more free program memory in our project. Unfortunately we
cannot use a processor with bigger memory. Do you have any easy…
Part Number: MSP430FR6820 Hi,
we are working on a design with MSP430FR6820, now trying to measure accurate values of thermistor, but It doesn´t work. Replaced termistor with fix resistors to check if ADC is counting properly; unfortunately counted values…
Part Number: MSP430FR6820 Hi,
we use the ADC module in MSP430FR6820 for two different measurements, having two configurations and 'deconfiguration' (common for both configurations).
We are doing the measurements in a cycle: first configuration…
Part Number: MSP430FR6820
Team,
For an MSP43 0 FRxxx + CC1xxx application:
It seems that for MSP43 2 the mbed TLS lib can be used: https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/795099 I know that TLS is suppose to use TCP/IP but I am looking…