Part Number: MSP430FR6928 Hi,
I use EUSCI UART_0 (9600 baud) and UART_1(19200 baud) for two different communication at same design. However, their interrupts effects each other and the datas are corrupted. If I disable one of them, the other one works…
Part Number: MSP430FR6928 Hi,
I am using DCO as main clock, not external oscillator. After power up, I am monitoring OFIFG bit is set. Is it normal behavior? Is it related with not using ext. oscillator?
Hi,
I am debugging the RTC_C function of the MSP4330FR6928 MCU in my project. I need RTC_C working in the counter mode. However, whatever I do, it is locked to the Calendar mode. I intend to generate 1Hz signal using the configuration. Unfortunately,…
Other Parts Discussed in Thread: MSP430FR6928 Hello,
I am using MSP430FR6928 Port 4.2 and 4.3 to perform UART TX and Rx function. The code is based on the MSP430 module library sample for eUCSI_A0. Please see the enclosed code. Voltage of the MCU power…
Hello,
I am developing software for a device based on MSP430FR6828 MCU using the sample code provided via the IAR Systems Workbench. I am trying to establish the I2C connection between the MCU and an EEPROM chip with an I2C address of 0x54. When the program…
Hi Bartosz,
I recommend using the MSP430FR6928 or MSP430FR6922 symbols as these devices have the same PM, RGC, and DGG package layouts as the MSP430FR6820.
Regards,
Ryan
There are signs that the following members are coming. Any hint when?
MSP430FR4131, MSP430FR4132, MSP430FR4133 MSP430FR5887, MSP430FR58871, MSP430FR5888, MSP430FR58881, MSP430FR5889, MSP430FR58891 MSP430FR5986, MSP430FR5987, MSP430FR59871, MSP430FR5988…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…