Part Number: MSP430FR6972 Other Parts Discussed in Thread: MSP430FR6989 Tool/software: Code Composer Studio Hello ,
I am making CAPTURE PROGRAM.
I am using MSP430FR6972 (I am making a pulse counter)
My intention is 1) to take the analog Value through…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Hi,
I have one simple question.
I am using MSP430 microcontroller with BLE5 module (UTO-NBL-52).
I am programming MSP430 ,
And then transmitting the value to BLE5 module (UTO-NBL-52)..
The…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Hello,
I have customized board of MSO430FR6972,
I am using UART0(UCA0TXD , pin No. : P2.0)
I transmit data with Baud rate 9600 bps,2400 bps, 4800bps.
The UART is working.
The Terminal used…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Hello,
I want to use Hardware Breakpoint,
I have Program made on CCS7.4.0.
I am using one MSP430FR6972 Board also.
I want to use Hardware Break Point (in Between the "UART" Communication )…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Dear team,
My customer used 2 UARTs(eUSCI_A0 , eUSCI_A1 ) of MSP430FR6972. Now they want to use UART BSL.
Please kindly tell me how to realize this function?
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Hello,
I am using MSP430FR6972.
I am using Intrinsic Sensor(in build in the controller that is " A30").
After making the program,
I am checking the sensor value.
My reference voltage…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Hello,
I want to use RF Module (400 MHz RF, NMT-UM434R1 fron NEO mobile technology).
I want use the module with MSP430FR6972.
But I am not getting any clue, how to use it.
And the data sheet…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio Hello,
I have problem with MSP430FR6972 , in the ADC program..
I am using two ADC( ADC15 & ADC30/integrated temp sensor.)
I take two values, in two different memories (ADC12MEM0 & ADC12MEM1…
Part Number: MSP430FR6972 When MSP430FR6972 is used, there are the following phenomena: 1) When the power is close to the reset pin, 430 will go offline to reset pin work during work, resulting in MCU reset;2) When THE NB module is close to the power…
Part Number: MSP430FR6972 Tool/software: Code Composer Studio I have used MSP430FR6972 with 424MH RF module.
It is a customized board.
Can you please tell me, how to check db value (ex: -20db).
Or can you please giver me any idea , how to do that.
Thanks…