Part Number: MSP430FW427 Other Parts Discussed in Thread: TIDM-WATERMETER-LCSENSOR For the selection of the inductor, my question just as the bellow:
does the Q value of the inductor infuence the performance of the SCANIF/ESI Module used in the water meter…
Other Parts Discussed in Thread: MSP430FW427 Hello everyone,
i want to use SW UART by using Timer A in MSP430FW427, i am able to transmit the byte but having problem in receiving a byte. P1.0 (CCI0A) is used as a transmit pin and P1.1(CCI0B) as a receive…
Other Parts Discussed in Thread: MSP430FW427 hi i am working on MSP430FW427 for water meter , this device does not haave UART module so, i need to use software UART , in example codes its working fine in eco mode but when it comes to string communication…
Studied the slaa341 application note. The uart used in this program is the controller's integrated usart. The MSP430FW427 controller does not have the built in usart, we have used a soft uart using timer A0. How do i change the assembly code for flash monitor…
Other Parts Discussed in Thread: MSP430FW427 Dear, I have below question about MSP430FW427 non-magnetic application:
1 . Whether the impact of the external magnetic field can interfere with the detection of the analog front-end 2. The consistency of the …
Other Parts Discussed in Thread: MSP430FW427 Hello,
According to the MSP430FW427 datasheet, this particular microcontroller has no native comms module (USCI module).
Has anybody ever written a software SPI for this microcontroller? Or alternatively,…
Hi Kai
I can't find the slaa138a in the on line. What I have saw before are two solutions in TI:1. MSP430FW427 http://www.ti.com/tool/TIDM-WATERMETER-LCSENSOR
This solution will be low cost than MSP430FR6989 with the SIF module but have less performance…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP430FW427 My customer is developing an electronic water meter based on MR reluctance elements.
They learned from the Internet that TI has a magnetoresistance solution chip MSP430FR6989, which…
Other Parts Discussed in Thread: MSP430FW427 , TIDM-3LC-METER-CONV , FLOWESI-GUI , TIDM-WATERMETER-LCSENSOR Hi,
Is there any design reference or code example for using the MSP430FW427 with 3 LC s in 120º ?
I know there is something like this for the MSP430…
Hello,
i'm using a MSP430FW427 and i have a similar question to this old thread (but with different mcu).
My clocks configuration is the following:
- MCLK = FLL
- FLLref = XT1
- XT1 = 32768 crystal
- ACLK set to be equal to XT1
- Timer B running with…