Other Parts Discussed in Thread: MSP430FW427 Hello, I have a problem.
In msp430fw427, after receiving some bytes, i'm save them into a flash.
And, i use scan interface.
My problem is after saving into a flash, programm goes in ISR for Scan interface…
Other Parts Discussed in Thread: MSP430FW427 Hello everyone,
I am using MSP430FW427 for ScanIF purpose. I am able to check the un damped and damped oscillations for 2 LC sensors but when i tried to check for 3 sensors, no oscillations were found.
My question…
Ricky Tangri said: I have already read TI's brochures (and the code examples) slaa222, slaa288 and slaa321.
Try slaa578. - Which by the way is first in the application notes list of MSP430FW427 product page.
Thank your for your speedy response I reviewed SLAA535a.pdf & SLAA535a.zip and I think I have a handle how to do this now. (although my MSP430G2231 is still in the mail) If I am correct once I have loaded "lpad_bsl_int.c" on to the MSP430G2231 and I…
Hi,
I read 4.1 but i am using only single sensor in my pcb(i.e., p6.0) . other sensor is not present. so i replaced P6SEL |= 0x03 to P6SEL |= 0x01.
Code is as below
// THIS PROGRAM IS PROVIDED "AS IS". TI MAKES NO WARRANTIES OR
// REPRESENTATIONS, EITHER…
Other Parts Discussed in Thread: MSP430FW427 Hi all,
I have a problem with TPS780300250. I am using it in order to power an MSP430FW427.
When I use the LDO, with an input voltage of 3.6V the current absorpted is 7 mA and the output voltage is fine, 3V…
Other Parts Discussed in Thread: MSP430FW427 , MSP430FG4618 Hello all,
I am currently working with the ESW427 dev board from Softbaugh (has the MSP430fw427 chip on it...no ADC). In order to get value from an analog input; I can hook up an external ADC…
Other Parts Discussed in Thread: MSP430FW427 I am using the MSP430FW427 at the moment.
From looking at the datasheet, only pin 6.7 serves as an analog input. Surely there are other pins that serve as an analog input correct? Or maybe I need to change…
Other Parts Discussed in Thread: MSP430FW427 , MSP430F2274 So I'm just experimenting with getting an interrupt to work correctly. My code is:
#include
"msp430fw427.h"
#include " intrinsics.h "
#define LED1
BIT3
#define LED2…
Other Parts Discussed in Thread: MSP430FW427 I'm working with the MSP430fw427 in particular. I just learned how to interface the LCD controller with the LCD panel on the Softbaugh development board.
As we know 7segment displays work best with numbers…