Other Parts Discussed in Thread: MSP430G2333 Hi,
I am using MSP430G2333 and tried example code in CCS to test msp430g2xx3_ta_uart9600.c, now i need to generate PWM signals on PIN 8, 9 and 12. Can you please guide me with sample code.
Thanks and Regards…
Other Parts Discussed in Thread: MSP430G2333 , TPA3116D2 , MSP430G2533 Hello All,
One of our customer wants to develop volume control application using MSP430G2333+TPL0102(Digital POT)+TPA3116D2. Volume will be controlled by push buttons.
For this solution…
ACLK (32768Hz) There are in addition to described as there is also built-in oscillator for external crystal. We think there is a specified frequency accuracy?
Best Regards,
Kozo
Other Parts Discussed in Thread: MSP430G2333 Question: How do I generate a controlled PWM duty cycle output for a Timer0_A3 Block#0 pin?
I need a controlled PWM duty cycle for the pin P1.5 shown below.
My pin on board is connected to P1.5 (MSP430G2333…
Other Parts Discussed in Thread: MSP430G2333 What is the min, max, and typical Input impedance on the 10 bit A/D converter input on the MSP430G2333? The datasheet (page 34) mentions the mux on resistance is typically 1000 ohms but does not mention the…
Alexis - OK so the temperature sensor is very low quality. It also sounds like there is no want from the factory to improve the sensor accuracy with multi-point calibrations like are done with MSP430's - which seems silly to even have the sensor available…
Part Number: MSP-EXP430G2 We are using an MSP430G2333 in our design. We have had issues with high sleep current at cold temperatures (minimum of -30 deg.C). Through further testing, we found that the source of all of this excess current at cold temperatures…
Hi Shai,
those device are not supported by the MSP group but a different group. This is why it doesn't show up in the comparison table.
Via wuick research I've found MSP430G2333-Q1, MSP430F2272-Q1,MSP430G2553-Q1,MSP430G2453-Q1,MSP430G2231-Q1,MSP430GF2252…
Part Number: MSP430FR2532 Other Parts Discussed in Thread: MSP430G2333 , , TLV809 Hi,
In our existing design with micro controller IC MSP430G2333 we were advised to use a Supervisor/Reset IC TLV809K33.
In our new Capsense design we will be using TI’s new…
Hi Daniel,
Please view the legacy MSP430 selections below that are automotive qualified (as denoted by Q1):
Generic Part Number
Q1 Datasheet
Frequency (MHz)
Flash (KB)
SRAM (KB)
GPIO
Timers (16-bit)
Brown Out Reset
USCI_A (UART/LIN/Irda/SPI…