Part Number: MSP430G2402 Other Parts Discussed in Thread: MSP430FR2111 Hi
Looking for low cost MCU with below requirements:
Minimum of 12 GPIO
0.5KB RAM
8KB/4KB ROM/FLASH
Minimum 256B Internal runtime reprogrammable FLASH
Minimum 1x16bits…
Part Number: MSP430G2402 Hello,
The MSP430G2xx supports External Digital Clock Source. When an external clock is input to XIN (P2.6), can P2.7 (XOUT) be used as GPIO?
Also, when I checked the data sheet, I found in the explanation of P 2.7 that the…
Part Number: MSP430G2402 Goog Morning TI community!
Today I have a question about programming FLASH memory's MSP430 processors.
I use some segments of the Info Memory as EEPROM to store data, so I write on it several times during the execution of…
Part Number: MSP430G2402 Good Morning TI Community!
Today I'm here to try to find an answer to an old question, posted in September, that didin't have an answer right now.
Here's the link of the previous discussion on TI forum.
What I want to…
Part Number: MSP430G2402 Goodmorning TI Community,
Today I write to You because of a strange problem with some elecrtonic board on which there is the MPS430G2402 processor.
After some work cycles the processor stops working well and gets lost.
The…
Other Parts Discussed in Thread: CC1101 Hi All,
Have been working with a board I designed with the G2402. All was going well for a couple of weeks until this morning. Made some changes to my code - primarily added the following few lines to the source…
Other Parts Discussed in Thread: MSP430G2452 I can not seem to have the SCLK signal held low when operating in the slave I2C mode. The I2C communications run fine, but I need to introduce a SCLK clock stretch when 'reading/writing' data. After detecting…
The USI is not much more than a shift register with baudrate generator. So implementing I2C on it is, well, challenging. But definitely possible and people have done it successfully in the past.
I don't know whether there is a I2 demo code available…
Pardon me,
I see you are using the MSP430G2402 with Launchpad.
I am unable to program the chip
Writing Memory Block ... not supported by this driver
Any pointers would be greatly appreciated
http://e2e.ti.com/support/microcontrollers…