Part Number: MSP430G2433 We are using MSP430G2433 in one of our board, which acts as startup micro. whenever power button is pressed micro is supposed to turn on other outputs.
we are seeing issue very rarely where this micro is not powering On. while…
Part Number: MSP430G2433
I have project which was released for MSP430G2433 2-3 yrs back. I had compiled using CCS7.3 .
Recently changed my laptop. I installed same version of CCS , but when i tried to import project i m getting compiler definition not…
Part Number: MSP430G2433 Hi ,
In our product ,due to some scenario some times msp430G2433 voltage drops to 1.8v and comes back
to 3.3V ,just few microseconds
,but msp430g2433 goes to hangout ,no response stays there. so we can operate our product for…
Part Number: MSP430G2433
It is possible to enable or disable brownout reset in embedded c software
Difference between lpm and brownout
How to enable or disable lpm in embedded c
Part Number: MSP430G2433
Im having a problem with one of your products, The MSP430G2433. When I set the port output register, the port input register is also set. This makes sense in the way your diagram is shown, but is however not so useful for the…
Part Number: MSP430G2433
I have a problem with the program I am currently working on. It is using assembly on the MSP430G2433. Whenever I try to write a value from RAM to one of the CPU registers a reset is triggered. When I debug manually I can see that…
Part Number: MSP430G2433
Hey, im currently trying to implement a time sensitive interrupt in a MSP430G2433 using Assembly. I wanted to know if it is possible to use the register addressing mode for peripheral addresses such as port and timer registers…
Part Number: MSP430G2433 Hi Team,
We have received a report from our customer that when the MSP430G2433 enters 'sleep mode' (LPM3) and then wakes up he gets short glitches on all of the I/O lines. There are 64u seconds low pulse on startup on all of…
Part Number: MSP430G2433 I have a program that samples for 50 ms on a 1 sec period (approximately). Uses LFO for timing and ADC10 for sampling.
50 ms -> sample continuously 950 ms -> stop sampling and enter LPM3 with timer running off LFO
When entering…
Part Number: MSP430G2433 Hi MSP Team,
I have a customer who would like to communicate with their battery gauge & charger from a MSP430G2433. I have found the SMBUS library on dev.ti.com and want to ensure that this is fully compatible with the MSP430G2433…