Part Number: MSP430I2030
Hi,
I am trying to develop a library that will be used by several MSP430 based projects, I will therefore need to declare some weak functions as placeholders in library code, then have them override in application code.
The following…
Hello Hiren, Please check MSP430Ware for this device for relevant example code. MSP430Ware can be found within TI Resource Explorer within CCS or at http://dev.ti.com . Below is a link to MSP430i2030 code examples. check out the PMM examples for different…
Thank you. Now I am using MSP430I2030 chip and it is mentioned that this chip can be used with the launchpad. http://www.ti.com/product/MSP430I2030/toolssoftware
However, it is unavailable in DIP package, hence, I have soldered the chip on an adaptor, …
Other Parts Discussed in Thread: MSP430I2030 I am using an MSP-FET430UIF debug interface and an MSP430i2030 chip. Initially, I tried burning the following code:
#include <msp430.h>
int main(void) { WDTCTL = WDTPW | WDTHOLD;
return 0; }
Everything…
Other Parts Discussed in Thread: MSP430I2040 , MSP430I2030 I'm new to the MSP430 and TI CCS - so sorry in advance if this is a basic question
I just purchased the MSP430i2040 Sub meter EVM p/n EVM430i2040S
The demo when connected to the my PC serial…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…