Part Number: MSPM0L1228-Q1 Hello forum,
I'm using this M0L1228 as a LIN slave, and the protocol has a LIN conformance test (LCT) validation that must be passed. To be precise, I'm having problems with the LCT test 7.2.1.2.1; basically, it requests that…
Part Number: MSPM0L1228-Q1 Good Day,
We are considering using the mentioned MSPM platform.
Could you provide what are the available DMIPS for this platform?
Thanks,
Maciej Czajkowski
Part Number: MSPM0L1228-Q1 Other Parts Discussed in Thread: MSPM0L2228 Hi team,
I am currently evaluating the MSPM0L1228-Q1 (M0L1228QRGERQ1) for an automotive-grade project and wanted to know does the MSPM0L1288-Q1 support RTOS.
Thank you
Part Number: MSPM0L1228-Q1 In the file SPIMSPM0.c, in the initHw() function there is the following code:
if (hwAttrs->csnPin && ((format & SPI_CTL0_FRF_MASK) == SPI_CTL0_FRF_MOTOROLA_3WIRE))
{
/*
* A CS pin was specified, upgrade the 3WIRE to a 4WIRE…
Part Number: MSPM0L1228-Q1 Hello,
how to calculate and define the settling error for ADC sampling time calculation?
And what's the sampling time criteria?
in datasheet page55, M0L1228QPTRQ1
Use the following equations to solve for the minimum…
Part Number: MSPM0L1228-Q1 Other Parts Discussed in Thread: MSPM0L1228 Hi TI expert,
I need the interrupt feature of the GPIO of the MSPM0L1228. Could you help me confirm if all the GPIO has the capbility to generate the interrupt (IRQ) to CPU?
Thanks…
Part Number: MSPM0L1228-Q1 Other Parts Discussed in Thread: UNIFLASH Hi Team,
Had a debug and we ended up getting stuck at the following point, there was a FLASH DED error when reading from the start of the 'OTP' section (board-specific configuration…
Part Number: MSPM0L1228-Q1 Hi TI Expert,
I want to generate the PWM from the timer TIMA0, TIMG0 and TIMG4 module.
I want to get your confirmation about the PWM.
If I want to generate 4 channels PWM from TIMA0, will them be related. Could I adjuet…
Part Number: MSPM0L1228-Q1 Tool/software: Dear Expert
For the 5V-tolerant open drain IO type does not have the output-high PMOS, pullup resistor, or clamping diode .
But it has a pull-down resistor and an NMOS .
I use ODIO as the TXD pin to connect…
Part Number: MSPM0L1228-Q1
Hello,
we use the MCU : XM0L1228QPTRQ1.
What's the min/max capacitance requirement for VDD and VBAT capacitors? Including aging, DC‑bias, temperature, and tolerance effects.
The datasheet only show the nominal value…