Part Number: MSPM0L1304 Hi,
I have a question about NRST pin.
The NRST pin is muxed with I2C0_SCL (PA1) for 16-pin
My customer is using the MSPM0L1304 16pin device.
The NRST pin is disabled by application.
However, MSPM0 must be able to receive…
Part Number: MSPM0L1304 Hello Team,
One of our KMM customer is working on Battery powered triggering device with MSPM0L1105TDGS20 (20 pin) . In their application, They wish to configure MCU with min current for extending Battery life. So they are looking…
Part Number: MSPM0L1304
Hi,
I have a question about I2C bootloader.
NRST pin is muxed with PA1 for 16-pin SOT package.
PA1 is required to use the BSL for I2C.
NRST pin must be pulled up to VDD and TI recommends connecting an external 47-kΩ…
Part Number: MSPM0L1304 Other Parts Discussed in Thread: UNIFLASH Hello,
I'm working with the MSPM0L1304, and trying to get the internal temperature sensor working. The calibration value I'm reading from Flash is 0x0000016B (decimal 363) - this is giving…
Part Number: MSPM0L1304 Hi
Now, we can order MSPM0L1304 preproduction and Only 32 pin package is in production.
Do you have the plan of in production date of MSPM0L1304SDYYR (16 pin package)?
Thanks,
GR
Part Number: MSPM0L1304 Other Parts Discussed in Thread: MSPM0L1303 , MSPM0L1305 , Hello experts,
On the MSPM0L130x datasheet and website, the operating temperature range of the S version of MSPM0L1303 is stated as -40℃~105℃.
www.ti.com/.../mspm0l1303…
Part Number: MSPM0L1304 Dear E2E Support,
In Chapter 20.1.2 of our TRM, we mention that it's possible to re-gain debug access to a device which contains software that disables the SWD pins.
Could you clarify the exact sequence, duration, etc...…
Part Number: MSPM0L1304 Hi everyone,
we are currently working with the MSPM0L1306SDYY.
In the datasheet, a 10uF cap is recommended for VDD vs. GND and 470nF are recommended for VCORE vs. GND.
We are interested in decreasing these capacitances…
Part Number: MSPM0L1304 Hi experts,
Regarding MSPM0L1304SDYY, please confirm the following statement on P15 of the datasheet.
(1) Connect CVDD and CVCORE between VDD/VSS and VCORE/VSS, respectively, as close to the device pins as possible. A low-ESR…
Part Number: MSPM0L1304 Other Parts Discussed in Thread: UNIFLASH Champs,
customer needs to dedicate one sector to calibration data and would like to ensure that once programmed, the sector will not be overwritten by mistake, even when the application…