Next, I set the jumper to J67 and obtained the log.
---------------------------------------- Debug opened on URT0 I2C Port 1 initialized as Master port I2C Port 2 initialized as Master port I2C Port 0 initialized as Slave port eeprom: Content validated Cal…
Here's a log from the device during boot:
DLPC7540EVM_UART_log.txt
----------------------------------------
Debug opened on URT0
I2C Port 1 initialized as Master port
I2C Port 2 initialized as Master port
I2C Port 0 initialized as Slave…
- I have done initialization. I am able to run single-core examples on the SoC and edit them (like the hello_world.c example).
- I will check out the IPC example once I get two projects running on separate cores. Currently I cannot build the example multi…
Hello, Aaron ,
I tried connecting the Front - end card. I also tried attaching a jumper to J67 and taking logs.
I have attached a photo of the state when connected and its log.
< Contents of log >
---------------------------------------- Debug opened on…
Hello Naveen,
Could you try having only the two cameras that you plan to use connected to the board and running the two camera pipeline previously shared?
There is a known issue where we see the CSI2RX SHIM DMA context channel 0 accepts all handled data…
Hi,
My goal in my new project is implementation of a multi-axis control system with a PMSM. The control loop must have the circular/linear interpolation capability. Can anyone propose me a suitable TI microcontroller for this purpose that can serve the…
Hi Shotaro,
This is a known issue where we see the CSI2RX SHIM DMA context channel 0 accepts all handled data. Due to the driver implementation, all of the other sensors are still streaming so when one (or a subset) of cameras in a multi-camera system…
Ok, That does answer some questions.
But, now I am having the issue where the M4 core does not get built. The RPRC file does not seem to generate/exist
**** Build of configuration Debug for project ipc_rpmsg_echo_am243x-evm_system_freertos_nortos *…
Part Number: CC1352P Hi All,
RF_postCmd(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent);
In this function, the parameter ePri is described as " Priority of this RF command (used for arbitration in multi-client systems…
Other Parts Discussed in Thread: PGA309 , PGA308 , MULTI-CAL-SYSTEM 2 questions.
1. My company bought a Multi-Cal-System Basic Starter Kit. The CD as suppled did not have the PGA309 software, only the PGA308 software. I was advised by tech support (online…