Part Number: OMAPL137-HT Other Parts Discussed in Thread: MSP430FR5739
Hi,
On our board, we would be using a fpga and omapl137-ht. Is it possible to daisy-chain them together?
I saw BSDL file is available for omapl137, so I assume the answer is yes. I…
Sajad,
Are you looking for an HT (high temp) omap processor? You have selected the OMAPL137-HT, and it directed the question to the High Reliability team.
If you are looking at catalog processors to accomplish this, you will have more options. Please…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAP-L137 , Tool/software: Code Composer Studio Hello.
In the datasheet for the OMAP-L137 figure 6-12 it clearly shows a flash connected to the processor's EMIFA using the open NAND flash interface…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: OMAPL138 I am trying to find out performance benchmarks for this dsp. Specifically I am looking for 1024 point Complex FFT (Radix 4, with reversal) Speed (in milliseconds) and required Cycles.
…
Part Number: OMAPL137-HT Tool/software: Linux Hi,
I would like to ask about the performance of USB on omapl137 platform. Reading the LSP 02.20 Linux Drivers Datasheet, I see that the max speed attained on CDC devices can be (table on pg 24) 36Mbps . Can…
Part Number: OMAPL137-HT Other Parts Discussed in Thread: SYSBIOS Tool/software: TI-RTOS Hi,
I'm trying to figure out a strange cache behavior.
#define Cache_Type_L1P ti_sysbios_family_c64p_Cache_Type_L1P #define Cache_Type_L1D ti_sysbios_family_c…
Part Number: OMAPL137-HT Hi,
. I read this wiki:
http://processors.wiki.ti.com/index.php/OMAP-L13x_/_C674x_/_AM1x_Schematic_Review_Checklist
When USB PHY is powered off while still connected to a powered-on host, the customer would notice leakage voltage…
Part Number: OMAPL137-HT HI,
I understand normally we use DSP to wake up the ARM by enabling it through LPSC module. Is there a way to reset the ARM again (using software) later during execution ?
Thanks,
AQ
Part Number: OMAPL137-HT Other Parts Discussed in Thread: CC2520 Hi,
I am working on a project for the high-temperature environment. I have read that OMAPL137_HT are designed for 175°C but when I want to purchase it, it is only available at 125°C.…
Part Number: OMAPL137-HT In the datasheet for this part, SPRS677B Revised February 2013, the wire-bond pads for the KGD die (pp 22-27) do not specify the second external I/F port (EMIFB).
The PTP packaged plastic quad flat pack does specify the pin-out…