Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Hello All,
I'm working on OMAPL138 custom board in that I want to configure gpio as below 10mhz frequency, Initially, I ran with Cpu clock frequency at 300Mhz.
For changing…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: TLV320AIC3106 , OMAP-L138 Hi,
I am using OMAPL-138 processor with DSP core, so in for Interfacing I want driver code of McBSP and Codec (TLV320AIC3106) for bare metal (NON-OS), If possible then…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAP-L138 Hello,
For booting DSP core of OMAPL-138 currently we are using JTAG. Please suggest another way for booting.
Thanks,
Lavanya
Part Number: OMAPL138B-EP Hi,
I'm working on OMAPL138 processor with DSP core, and I want SDK for bare metal for all interfaces.
Please any one share me the link to download the SDK setup.
Thanks,
Nayan
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Hello,
I am working on OMAPL138 DSP processor, in that for interfacing I want codes for uPP, HPI and DDR2 in bare metal.
Can anyone Please provide these codes.
Thanks,
La…
Part Number: OMAPL138B-EP Hello,
I am trying to understand the meaning behind the Q4 suffix in PN OMAPL138BZWTQ4. Can you please assist here?
Thank you
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 MCU: OMAPL138 ;CORE: Linux-3.3.0 , U-Boot 2012.04.01-00054-g9a6dfff ,and mcsdk_1_01_00_02_setuplinux.bin
question1、when write the system to Nandflash ,device will sign below error and system cannoy…
Part Number: PROCESSOR-SDK-OMAPL138 Hi,
I got the following error when I was running McASP project.
xdc.runtime.Main: "src/mcasp_drv.c", line 4181: assertion failure
And the line 4181 is: assert(0U != timeout);
Can you let me know what the issue…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 Hi, I am working on the Universal Parallel Port driver for OMAPL138, I am not able to test the driver on the OMAPL138 board, if any way is there to test the driver, please let me know …
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 Hi TI
We will use DSP OMAPL138BZCED4 to develop our product, the picture is about PLL_VDDA filtering circuit we used, does it will be work OK for PLL?
Thanks!!!