Part Number: ONET4201LD Other Parts Discussed in Thread: DSLVDS1001 According to the datasheet of ONET4201LD, DIN+/DIN- are CML-IN.
However, the output of FPGA is COMS.
Therefore, I need a converter, which can convert CMOS to CML-IN.
Would you please…
Part Number: ONET4201LD In the data sheet, the differential input signal is 200 mVpp or more, but if I input a signal of 200 mVpp or less, will the output of MOD-/MOD + stop?
Or, the value of the output voltage is not guaranteed, but will some voltage…
Part Number: ONET4201LD Other Parts Discussed in Thread: ONET4201PA , Hi,
Do you any plans to develop a combination product of ONET4201LD and ONET4201PA like as MAX3710?
Best regards, Kato
Part Number: ONET4201LD Other Parts Discussed in Thread: ONET4201PA , I am new to DFB and FP laser designs. I am designing an SFP like product. Do you have any reference designs using ONET4201LD and ONET4201PA? On the RX side I would be using a PD. It is…
Part Number: ONET4201LD If there is no load connected to the MOD+/MOD- terminals, or if a high impedance load is connected to the MOD+/MOD- terminals and the maximum output voltage level (IMod=80mA) is set, is there any problem or danger?
For example…
Part Number: ONET4201LD I am following figure 24 in the datasheet in my design. Figure 24 shows a LD's anode common with PD's cathode.
But I really need to drive this laser (QLD-1550-40S) . Unlike the application in figure 24, this laser has the…
Part Number: ONET4201LD Hi team,
Datasheet describes that the output is optimized for 20ohm of load impedance.
Is it able to drive 50ohm load (100ohm diff) with ONET4201LD? Is there anything should be care when 50ohm(100ohm diff) load is driven with ONET4201LD…
Part Number: ONET4201LD Hiii
I want to use this ONET4201LD IC to drive my laser at 1Gbps.
Please find the attached datasheet of laser and let me know whether i can use the same IC or can you suggest some other better performance IC to drive the Laser…
Part Number: ONET4201LD I'm currently using ONET4201LD and for future evaluation in different conditions and maybe different lasers I'll need to have different resistor values.
I'm wondering if there is a way of controlling that digitally... will…