Part Number: OPA2180 Other Parts Discussed in Thread: OPA2377 , OPA2376 , OPA2188 , , OPA2325 , OPA2397 , OPA2392 , OPA2387 , OPA2182 , OPA2187 , OPA180 , OPA188 Hi experts,
Q1. Could you please tell me your recommended devices that is alternative…
It should be possible to create a footprint that allows both MSOP-8 and DGK; even a standard footprint might work. (PW would be even wider.)
Looking at the electrical characteristics, the OPA2377-Q1 would be a better match.
Only the "MAX" values in the datasheet are guaranteed.
The TLV9062-Q1 is a low-cost device. There is no exact replacement for the RS722P. Other low-cost devices would be OPA2377-Q1 or LMV772-Q1; devices with similar or better characteristics in the…
Part Number: LMV342 Other Parts Discussed in Thread: TINA-TI , , OPA2377 Tool/software: TINA-TI or Spice Models Hi team,
Please let me ask you three questions regarding the simulation results of stability(Gain=1) and output impedance. In addition, I…
Hello Matthew-san,
I simulated the frequency response of the output impedance for LM1875. I'll attach the simulation file, the schematic and the result below.
6403.LM1875_zo.TSC
Looking at this result, I think that is not normal.
Checking…
HY,
Only TLV2197-Q1 and OPA2192-Q1 meet your 10MHz GBW requirement for automotive applications but if you absolutely need IQ of less than 0.8mA, please take a look at OPA2376-Q1 and OPA2377-Q1.
Hello Ilya,
Our precision operational amplifiers do not feature the ability to withstand a 32 V input over-voltage. The internal ESD protection is part of the reason and the other being that wasn't a design criteria. In many cases a simple input current…
Hi Kai-san, Marek-san
Thank you for response.
Kai-san
I will send your response to my customer.
Marek-san
Your answer is about opa2377-Q1.
I want a opa377-Q1(DBV Package 5-Pin SOT23) answer.
Could you tell me ?
Best Regards,
Koji…
Hi Frank,
Can you elaborate on: "When we plug in the phone line and very high freq ringing couples onto the 5v power supply".
Does the supply peak above 5.5V? What is the "high frequency ringing"? Is this the ~20Hz phone line ring freq coming through…
Part Number: TLC555-Q1 Other Parts Discussed in Thread: TL431-Q1 , OPA2377-Q1 , NE555 , TLC555
Hi,
Customer would like to use TLC555-Q1 for oscillator about 100Hz~200Hz.
It has to used in full thermal range so tolerance is important.
In the datasheet…