Part Number: PCA9534
Tool/software:
Hi TI
I am using PCA9534DW and PCA9534A
But there are two kinds of marking
"1CC821T PCA9534"
"23C1EJT PCA9534"
I would like to ask what the difference between the two markings is
(I want to know…
Part Number: PCA9534A Hello,
In the data sheet, page number:16 it was mentioned that "Resetting the interrupt circuit is achieved when data on the port is changed to the original setting, data is read from the port that generated the interrupt."
…
Part Number: PCA9534A Other Parts Discussed in Thread: TCA9534A Tool/software: Hi, I understand this is rather an old but very common part. Is there any EOL plan for this part and if there is, will there be an drop-in replacement? As the recommended new…
Part Number: PCA9534A Other Parts Discussed in Thread: PCA9554A , TCA9534A , TCA9554A , TCA9534 Hello,
I am using 3x PCA9534A IO expanders and sometimes the device will hold the SDA line low at power up. All that is on the bus is a micro controller…
Part Number: PCA9534A Hey, we tend to use this device on our board.
In a case of write operation, when the master send the command byte wrong with a sixth 6 MSbits other than zeros ("0") how would the slave acts?
For example instead of 0x03 it sends…
Part Number: PCA9534A Hi team,
My customer is using our PCA9534A ,and they find when they config 0 x03 ,the value read and wrote is not the same.
They also check the input register 0x00 ,they find the value also can't match the input voltage.
Could…
Part Number: PCA9534A Dear Sir or Madam,
I am having problems getting communication with the PCA9534A.
I see the CLK and SDA lines are pulling the commands on the i2c bus low in the correct way. the same circuit work when implemented on a different…