Part Number: PCF8574A Tool/software: Attached is a diagram/doodle of the circuit being used. Conditioning components are mitigated for simplicity but they all conform to datasheet recommendations for filtering and the like. The PCF8574A is being used…
Part Number: PCF8574A Other Parts Discussed in Thread: TCA9539 , TCA8418E Tool/software: Question:
I'm using the PCF8574A I/O expander in a project and encountering an issue with its interrupt (INT) line. The device generates an interrupt on any rising…
Part Number: PCF8574A Other Parts Discussed in Thread: TCA9534A , TCA9534 , , PCF8574 Tool/software: Hello, I am using PCF8574ADWR connected according to the attached diagram. After sending data to the output, there is no data on the outputs, despite…
Part Number: PCF8574A Other Parts Discussed in Thread: INA138 , ADS7830 Tool/software: Dear All,
I have to interface your PCF8574APWR with 74HC4051PW .
In particular:
Both pin will be powered at 3,3V
the PCF P7,P6,P5 will activate the control…
Part Number: PCF8574A Other Parts Discussed in Thread: TCAL9539 Tool/software: Hello,
we are considering using the PCF8574A Remote 8-Bit I/O Expander and reading the datasheet following questions came up:
Is it allowed to have 3V3 on the P[0..7] IO…
Part Number: PCF8574A Hi,
I am trying to use the IO expander chip PCF8574A to READ ports P5-P7.
I do not have any devices connected on these ports, the pins are just pulled up or pulled down so that they return either 1 or 0 (these help with binary…
Part Number: TMS320F28379D Other Parts Discussed in Thread: PCF8574A , C2000WARE Tool/software: can you post what are i2c configurations you have used for interfacing PCF8574A and sample code of it for reference?
Part Number: PCF8574 Other Parts Discussed in Thread: , TM4C129ENCPDT , P82B715 I am writing to PCF8574 and PCF8574A devices using the TI driver under TIRTOS.
TM4C129ENCPDT processor, latest TIRTOS available for this processor is being used.
The…
Part Number: PCF8574A Hello,
I have seen several posts like this for using PCF8574A to use the Keypad as an I2C peripheral. Some of them are using pullups for the columns and others don't. I have attached my design and I would appreciate the feedback…