Part Number: PCM3008 Dears:
From our datasheet of PCM3008 it will generate some noise and according to test it happens indeed, could we use some method to avoid the click noise?
Since we will use PCM3008 to replace AK4554VT.
Pls. kindly give some advice…
Part Number: PCM3008 Dears:
Could you kindly help to give some information about PCM3008T's Life Circle?
Since our customer will use PCM3008T to replace AK4554VT, however, customer want to know the Life Circle to decide to use our solution.
Or you…
Part Number: OMAP3530 Other Parts Discussed in Thread: TMDSLCDK138 , PCM3008 , Hi experts,
Q:Is there any problem if we connect an oscillator (Square) of ±30ppm at 4.096MHz to McBSP_CLKS?
There is no provision in the datasheet regarding the tolerance…
Other Parts Discussed in Thread: PCM3008 According to the datasheet, the PCM3008 is capable of sampling rates from 8kHz to 48kHz. I have been unable to use the device at sampling rates less than 16kHz without generating significant noise out of the DAC…
Other Parts Discussed in Thread: PCM3008 Hi,
i'm trying to connect pcm3008 code to pic18f46k22.
Somebody knows what is the LRCK pin in the pcm3008?
I can't understand where to connect that pin in the pic.
maybe somebody have some code for this…
Other Parts Discussed in Thread: PCM3008 Hello All
Im making an audio sampler using a TI PCM3008 and an STM32 microcontroller.
I am using the recommended circuit from the datasheet but Im not sure if i can send audio straight in or if I need to condition…
Hello,
There is not an available IBIS Model for the PCM3003. There is one for the PCM3008 which was from a similar time period and can be used a good baseline for how the PCM3003 digital interface will operate.
Note that while these devices are still…
Hi,
You can refer to the attached excel for a high level summary of these parts.
AIC3254 driver should work with the PCM3070.
8838.AIC-PCM products.xlsx
Regards.
Hi Yuki,
I have attached here our CODEC products for you to peruse, you can click the part number to go to the product folder.
Take a look which will suit your customer requirements, these are currently active devices.
Let me know if you have other question…
Thanks for quick reply.
With yocto build image, I have, it provides PCM3008 drivers which looks more similar to PCM3002 except that it does not show I2S interface when looked at datasheet. Do we have any interfacing example of PCM3008 Audio codec? Or…