Part Number: REF2033 Hello,
May I have the schematics model and footprint of REF2033 for altium designer? It was not included in altium's library files for TI voltage references.
Thank you,
Handenur
Part Number: REF2033 Other Parts Discussed in Thread: TLVH431 Hello
I have an ADC driver. the supply is 5V and the Vcm (common mode voltage) should be 1.65V.
usually the common way to provide the Vcm is, using a voltage divider with two 1K resistors…
kai klaas69 said: the REF2033 needs more input voltage than VREF+10mV to regulate properly.
REF2033 regulates the input voltage very well until PWM is running for the DC inverter. checked again and the 3v3 LDO (TPS73533DRVR) is providing the REF2033…
Part Number: TIDA-010232 Other Parts Discussed in Thread: TLV6001 , REF2033 , AMC3330 Tool/software: ok, its been a long day, so I apologise if I'm asking stupid questions, but...
Following the implementation of "electric bridge method" of insulation…
Part Number: LMR14203 Other Parts Discussed in Thread: REF35 , REF2033 Tool/software: I am looking to have a negative Vout using the LMR14203. I am looking to step down 30V at Vin to -5V at Vout. I tried using the power designer tool to create a topology…
Part Number: LM4128 Other Parts Discussed in Thread: REF4132 , REF2033 Tool/software: I'm considering LM4128's enable pin control by logic IC. I want to know LM4128 enable pin's input impedance or input leakage current.
Please let me know. Best regards…
Part Number: INA240 Other Parts Discussed in Thread: REF2033 , INA500 , INA170 , INA132
Tool/software:
Hello experts,
We are looking for a (preferred)single chip solution , which does the following, with one major change.
The differential inputs…
Part Number: MSP-EXP432E401Y Other Parts Discussed in Thread: REF2033 , MSP432E401Y , Good evening, I hope all is well!
I am working on a circuit, and I have run into a question. I am using the REF2033 to create a reference voltage of +1.65V, and will…
Hi Vaibhav,
Yes, change the reference voltage to 3.0V/1.5V would be a simplier way. Just replace the U11 of REF2033 in this reference design to a REF2030 will do.
Best regards,
Jerome Shan