Thank you for the answer.
I am planning to use multiple LMX2572 devices in a phase-coherent multi-channel RF system. My intended RF output frequency range is in the L-Band, hence I need to use channel divider with the division ratio other than 1 to…
Hi, so just to confirm:
Of course we will evaluate the IWRL6432 vital signs demo. Two questions before we commit:
1. Does the IWRL6432 vital signs demo use the same breathing rate estimator as
the 6843 demo? We ask because the limitation we reported…
Evan, thanks! Is there a practical max output swing range(at high load resistance) that we can achieve? That would be helpful for the reasonable input common-mode range estimation in our application.
Hi Anil,
Here is a measurement with:
CH1 Vshunt (0.39ohm) serial to transformer
CH2 transformer primary voltage
CH3 / CH4 VGS SR E&F
Vin 390V Vout 40V Iout 6A
TI UCC28951 Design Tool.xlsx
I also noticed that the frequency and amplitude…
Hello,
Thank you for reaching out. Can you please share more details around the project you're working on with our AFE7769D?
Application (repeater, small cell, etc.):
Use case (include RF frequency, IBW, output power level):
Timeline to board…
Part Number: MMWAVEPOEEVM Other Parts Discussed in Thread: IWRL6432AOPEVM , IWRL6432AOP , IWR1843 , IWR1642 Hi TI team,
We are evaluating TI's mmWave radar devices for a high-speed proximity sensing application and would appreciate some guidance regarding…
Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: IWR6843AOP Tool/software: Similar questions to the related post
Is this present in the out of box demo for IWR6843AOP?
The release notes mention that "slope error of 1-bit can cause errors…
Thank you for the reply. Since going through the RTOS based code with many functions applicable to motion detection takes lot of time, how i can build range estimation application in no-os application with set of required functions. Please give the quick…
Part Number: IWRL6432AOPEVM Other Parts Discussed in Thread: IWRL6432AOP Whether we can check the mmwave radar range estimation performance in semi anechoic chamber. Since to have the performance measurements for fixed targets, we checked the range estimation…
Part Number: CC2340R5-Q1 Hi Team,
We are using the CC2340R53 for a BLE design and are performing antenna/matching-network simulations in ADS.
Could you please provide the following:
S-parameter (.snp) model for the CC2340R53 RF path, covering…