Hi Rogelio,
Under Japan's Radio Act, certification testing evaluates RF emissions purely based on declared frequency range and data rate, regardless of the Bluetooth protocol's own channel usage rules. If we declare 2Mbps operation across 2402-2480MHz…
Part Number: TPA3116D2 Dear TI Support,
I am currently evaluating the TPA3116D2EVM with a 24 V power supply.
I would like to ask about the TPA3116D2:
I could not find a clear specification in the datasheet regarding the input voltage range for the…
Hi Ali,
I tried to download the pdf file above and successfully downloaded it. Please try this one. Brief Design and Functional Outline - WFOV (2).pdf
Regards,
Danilo
Part Number: IWR6843AOP Other Parts Discussed in Thread: IWRL6432AOP We are using devices IWRL6432AOP and IWR6843AOP for our application.
we have installed CCS 20.05.01 and installed SDK for both devices,
SDK XWRL68XX-3.2 is installed for IWR6843aop…
Hi Yvan,
It looks like the LM337-N model was reused for the LM337 - the model file you attached matches the LM337 exactly.
Unfortunately, this model uses an older model architecture which does not support operation with the input voltage outside of…
Hi Tony,
Thanks for your reply. Currently, customer see that the rated temperature of this inductor is around 155°C. If the actual measured inductor temperature is around 130°C with this type of package, should we also consider the potential impact…
Hello,
The general purpose of measureRangeBiasAndRxChanPhase is to measured while in an anechoic chamber with only a corner reflector. This way we sort of "benchmark" the core RF analog components and make offset adjustments as necessary. The sensor…
Hi Mike,
Could you provide the values of the feedback and gain resistors? To calculate the output power dissipation, I'll need these values to determine the effective load resistance.
With a maximum operating ambient temperature of 90C, the maximum…
Part Number: LMX2582 Other Parts Discussed in Thread: LMX2491 Dear TI Technical Support Team,
I am currently developing a signal source based on the LMX2582 wideband frequency synthesizer, targeting an output frequency range of 2.4 GHz to 2.5 GHz. The…
Dear Sir/Madam,
We have an additional inquiry regarding how to display SOH (State of Health) in the user interface.
We are considering two possible methods and would like your recommendation:
Displaying SOH as a real-time percentage value (e.g…