Hi Dale Li,
Thank you for the clarification.
For our formal worst-case error budget, we would like to confirm one additional point.
The ADS124S08 datasheet specifies a minimum DC CMRR of 110 dB.
Can we use this guaranteed minimum DC CMRR specification…
Hi Carrie,
Thank you very much for your kind support.
Our application is an optical shutter control system using a piezo actuator. Based on our current estimation, the minimum rise time is around 2 ms, and we may adjust it to approximately 2.5 ms…
Hi srinivas,
It appears that your board has a JTAG header, is it possible to connect your board to SmartRF Studio 7 and test the range of the IEEE PHY? If it is similarly poor then it is likely a HW issue, but if the range improves we will need to further…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: AWR2243
Tool/software:
Hi,experts:
I want to observe the IQ mismatch phenomenon from the mmwcas-rf-evm,the version is PROC054 REV-E,i'm using mmwcas-rf-evm + mmwcas-dsp-evm to capture the…
Hello Hitesh,
Thank you for the updated details. Yes, your method and values are correct for the OPA857.
For the THS4541 resistor and VOCM values, do you happen to know the ADC in STM32 MCU's full scale range and input common-mode voltage? The full…
Part Number: ADC12D1800RF Other Parts Discussed in Thread: ADC32RF55 Hello TI support team,
I would like to check if TI offers any ADCs that are explicitly specified to accept direct analog I & Q baseband inputs (i.e., separate analog I and Q channels…
Hello Jaydeep
Can you share more details on the application and what is the end equipment here?
Vin range
Vout
Iout max
Additionally, I would recommend filling out QuickStart calculator available on product page, this will help you understand…
Hello Tommy,
I am sorry for the delay on your questions. Below includes feedback on your list of questions:
The IN+ pin of the amplifier is set to VBIAS of 250mV because the amplifier is in single-supply configuration, and amplifiers, even if rail…
Part Number: LMX2592 Other Parts Discussed in Thread: , LMX2595 , LMX2594 , LMX2572
Hello TI team,
I am planning to use the LMX2592 as a replacement for the Analog Devices HMC832 (PLL + integrated VCO) in an existing radio system. I would like to…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: UCC12050 , Hello TI team,
We are designing a per-channel isolated 4–20 mA input board, with a normal measurement range of 0–24 mA.
Our proposed circuit is: - External loop -> TPS26610 (candidate…