Part Number: LMH2120 The datasheet provides some useful information regarding the relationship between the RF power recorded and the LMH2120 output voltage at different frequencies (e.g. figure 2, figure 32, figure 41, etc) - however I only see the data…
Hello Chris,
Thank you for the simulation.
If I understand you correctly, in your simulation — with no intentional DC at the input source and without any AC coupling — the output of the charge amplifier goes into positive saturation . If that is the…
Part Number: LMG3522R030-Q1 Hello TI Team,
We are evaluating the LMG3522R030-Q1 for a high-frequency power converter application with a switching frequency in the range of 300 kHz to 500 kHz .
The datasheet specifies the VDD operating current as 15…
Hi,
The level sensing demo performs zoomfft after range fft. As a result accuracy provided by the demo is 1mm. Even if you reduce the range step, accuracy after the zoomfft will not improve.
Range resolution can be increased by utilizing the entire…
Part Number: LMX1204 Tool/software: Dear TI Engineer,
We need an RF mixer with an IF/RF frequency range of 1-4.5GHz, and the LO frequency band is between 1-3GHz. Do you have any recommendations for this requirement?
Thanks,
Kind Regards
Hello Phil
Operating junction temperature range for the device is –40°C to 150°C as mentioned on page 1 and 4. The range mentioned on page 40 is ambient temperature range. Although, for more accurate estimation of Ta for the device I would recommend…
Part Number: BQ27742-G1 Other Parts Discussed in Thread: GPCCHEM Dear TI Support Engineer,
I am using a BQ27742-G1 for a single-cell Li-ion battery.
The battery manufacturer specifies a nominal capacity of 3130 mAh at a maximum charge voltage of 4…
Part Number: UCD91320 Hi Team,
Currently using UCD91320 for voltage margining
How should the following parameters be set?
VOH : ?
VOL : ?
F_CLK : ?
When adjusting the voltage margin, should we use DPWM VOH or DPWM duty cycle?
According to…
The demo at run time will provide some error information that is sent to the visualizer through the UART. This is the message you see in the Visualizer.
For more information, one should connect CCS debugger and check where the demo fails.
In this…
Hi Manikata,
The synth may not lock when using the CC1125 outside of the frequency ranges listed in the datasheet. However, the reason these ranges are stated is because this is what the VCO tuning range supports.
From Section 9.12 of SWRU295 ( CC112X…