Hi, there:
For AWR device, boot loader may initialize some of the memory to zero. For IWR device, the memory is not initialized. The users will need to take responsibility to initialize/program these memories.
For the HWA parameter sets configuration…
Hello Hari,
Here is some feedback on our end as well:
Current source: Analog current source from an IR LED? If so, then:
Is input capacitance estimated to be around 1.3pF for intended reverse bias voltage from your schematic?
What is estimated…
Hi Rushikesh,
From the images you attached, I can see that the S3 switch positions for Flashing Mode and Functional Mode are inverted. Please follow the steps below:
1. Set S3 to ON (Flashing Mode) and flash xwr68xx_mmw_demo.bin using UniFlash. Check…
Hi,
Please see my response below. What is the specific inter-op issue you are having?
1. TMDS Clock Counter Registers & Frequency Conversion Formula (EyeScan Equivalent)
We need to measure the actual frequency of the incoming TMDS clock to choose…
Part Number: CC1310 Tool/software: Sir/Madam,
We are currently working on a wireless communication project involving two different platforms:
TI CC1310
STMicroelectronics STM32WL55
Our aim is to establish communication between these…
TTD,
The common mode limitation and output swing limitation are mostly independent ant of the power supply. For example, Vicr is specified to be -15V to +13.5V on a ± 15V supply. This means that the common mode range is valid all the way to the negative…
Hi Board Designers,
Inputs related to thermal data/pictures for a given system design (SK or EVM)
We do not provide thermal data but instead we provide customers with technical resources to assist their thermal analysis. Please note, our EVMs typically…
Hi ttd,
The TUE calculation is a very conservative estimate for error. When we include the number in datasheets this is an actual measured value on the device. In reality some errors may be positive while some are negative, and they'll end up cancelling…
Hi Adrian
I am referring the pdf for the calculations. I even made an Excel which calculates these things.
I have feed the data as per your suggestion in mmWave Sensing Estimator and calculated back Max Range, Range Resolution ,Max Velocity and Velocity…
Part Number: AWR2243 Tool/software: Im using MMWAVCAS-RF-EVM with MMWAVCAS-DSP-EVM (AWR2243's) with mmwave_studio_02_01_01_00, using 4chip MIMO cascade mode.
We would like to test it at approx. 130 meter max range.
Do you have links to a longer range…