Bonjour, je travail avec la carte MSP432P401R. Cependant, je dois concevoir une interface graphique avec la bibliothèque LVGL mais j'arrive pas à télécharger le Plugin au niveau du site ti.com. Pouvez vous m'aider à résoudre mon problème.
Part Number: SIMPLELINK-CC13XX-CC26XX-SDK Other Parts Discussed in Thread: CC1352P Tool/software: Hi.
I want to create the project which is rxAudioTx example at launchpad CC1352P.
When I create the example, I got the error message below:
Project…
Hello,
Shivaji Nawatakke said: 1. I wanted to develop the Graphic application on the MSP432P401R first on the Launchpad red 2 and then, on our own custom board. I came across the nice example in the SIMPLELINK-SDK-LVGL-PLUGIN _3.30.00.06. Which I wanted…
Part Number: SIMPLELINK-MSP432-SDK
Tool/software:
Hi,
I am using MSP432P401R with FreeRTOS.
For most work, I need to use the SDK and driverlib. It works fine when I use example projects from the SDK.
But when I use FreeRTOS example projects…
Part Number: SIMPLELINK-WIFI-TOOLBOX
Tool/software:
On Linux (Ubuntu 24.04), one is forced to pollute /usr/lib , which is not meant to be manually modified by the user.
Instead, the $HOME/.local/lib/wireshark/plugins directory should be supported…
DONGHYUN LEE said: I downloaded the SDK directly from ti.com and ran the installer.
I will bring this thread to the attention of the team responsible for the SDK. They can assist further.
Thanks
ki
Part Number: SIMPLELINK-CC13X2-26X2-SDK Other Parts Discussed in Thread: CC1352R Tool/software: Hi,
I am currently reviewing the Bluetooth Core 5.2 qualification tests for CC1352R in the bluetooth qualification workspace.
https://qualification.bluetooth…
Part Number: SIMPLELINK-CC13XX-CC26XX-SDK Other Parts Discussed in Thread: SYSCONFIG Hello,
My customer uses CC2642 and recently moved from SDK v6.10 with IAR v8.50.5 to SDK v6.30 with IAR v8.50.9. Now the TI-RTOS plugin doesn't work anymore in IAR…