Part Number: SN54AC244 Hi,
I have the need to add a pullup on OE for one mode on my board design and to add a pulldown on the OE on another mode of my design such that one mode the driver won't be active and in the other mode the driver will be active…
Part Number: SN54AC244 Dear TI experts,
According to SN54AC244 datasheet, there is only SNJ54 and SN74 ordering number.
There is no SN54 series. But the title is SN54AC244.
I want to find SN54 series information.
Are they same parts SN54 and…
Part Number: SN54AC244-SP Hello,
I am trying to find the thermal impedance of 5962-8755201VSA? Is there any information on this. I cannot seem to find the information in the datasheet. Also, what occurs when the max junction ambient is reached? Is there…
Part Number: SN54AC244 Hi Team,
My customer would like to know the thermal data of SNJ54AC244 CFP(W) package. Complete thermal data (theta JC, JA, JB, etc.) is much appreciated.
Looking forward to your reply.
Regards,
-Renan
Part Number: SN54AC244-SP Other Parts Discussed in Thread: SN54LVCH244A-SP I am using two parts that TI's datasheet states are qualified for space: SN54AC244-SP (SMD 5962-8755201VSA) and SN54LVCH244A-SP (SMD 5962-9754201VSA). The datasheet goes on to…
Part Number: SN54AC244-SP It was not clear from the datasheet whether the data and control inputs can handle 5V inputs when VCC is 3.3V without damaging the part. The absolute maximum ratings includes a Note 1 that says: "the input and output voltage…
All CMOS devices allow their outputs to be paralleled; see [FAQ] Can I connect two outputs from a CMOS logic device together directly?
You can use bus-hold inputs in parallel if the other device has enough drive strength. If in doubt, put another buffer…
Hi Wade,
Thanks very much for the additional info, the link had some good info I will want to fully digest.
To make sure I understand: When you say my estimated Ron will be pessimistic, your saying it Ron is likely lower than estimated? For example…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…