Part Number: SN55LVCP22A-SP 5 years ago on this forum it was indicated "Our team is working on publishing the SEE report to the product folder. We have preliminary data though, and can provide some slides after crunching the data."
The datasheet for…
Part Number: SN55LVCP22A-SP Tool/software: Good morning,
we selected TI PN SN55LVDS32W for the Leo PNT solution we are designing.
We are trying to understand / estimate the isolation level of the two clock paths that will be managed by the device…
Part Number: SN55LVCP22A-SP Tool/software: Hi,
Per Figure 6-2, for 25C, the supply current as a function of frequency is relatively flat, sitting around 60mA. Per datasheet section 6.5, the quiescent current is 60mA (TYP) and 87 mA (MAX). Typical values…
Part Number: SN55LVCP22A-SP Tool/software: What should be done with unused LVDS inputs on this part?
Section 9.2.3 describes an unused single ended LVPECL input, but there isn't any recommendation for an unused LVDS input pair.
Part Number: SN55LVCP22A-SP Tool/software: Hi,
On page 20 (section 11) of the SN55LVCP22A-SP datasheet, there is a layout example for this part. I was wondering if there was any significance to the lengths of the traces for each pin according to the…
Part Number: SN55LVCP22A-SP
I have a question while using SN55LVCP22A-SP part. In the figure below, how many volts should VCC be applied to make VOS 1V?
Part Number: SN55LVCP22A-SP Tool/software: I’m using a SN55LVCP22A-SP as a splitter. What do I do with the unused differential input? I’d assume I float it but what’s the recommended connection?
Part Number: SN55LVCP22A-SP Hello. We are in need of the PSpice model for the SN55LVCP22A-SP component for our project. Could you please provide us with this model at your earliest convenience?
Thank you.