we do not have the completely integrated version but we have device with integrated transformer drivers that only require an external trnsformer and an LDO.
These new devices are ISO1176T, ISO3086T and ISO35T.
we also have a new miniature EVM featuring…
Hello Yuyama-san,
Please see attached. Please not that not much was changed, Rev B is to incorporate the AMC1336 device revision on the same board. sbau271.pdf
Part Number: AMC1100 Dear TI team,
Good evening.
We are measuring AC voltage of 50KHz switching frequency and fundamental frequency of 50Hz at input side of AMC1100,which is very noisy.(Kindly find the attached images of waveform.doc)
We are not…
Other Parts Discussed in Thread: TIDA-00555 , AMC1100 , AMC1100EVM , ADS7263 Hi,
My name is Idan and I'm electronic engineering at the Israeli Aerospace Industry.
In my application I have I have to use isolated shunt resistor in order to measure the…
Hi Ali
Thanks for the reply.
1. I am using ISO1050EVM CAN transciever.It has 120 ohm terminating resistance.Here is the datasheet:
user guide.pdf
ISO1050.pdf
2.I am using oscilloscope to observe the waveforms-CANH/CANL/TXD pins and all.…
Hi Tom,
Please find the attachments, that include Schematic and PCB layout. we are using the same isolated power supply used in AMC1311 EVM ( http://www.ti.com/lit/ug/slau745/slau745.pdf )
5V isolated supply design diagram.
reference diagram…
If your truly interested why 1/2 LSB settling even though it seems an MSB issue, PDF below link is an excellent 2018 source.
/cfs-file/__key/communityserver-discussions-components-files/908/TI_2D00_Analog-Engineers-circuit-cook-book-slyy138.pdf