Part Number: SN65C1168E-SEP Hello,
On the data sheet for the part listed above, I've found the theta JA thermal impedance listed. However, I was wondering if you could provide a representative junction-to-case or junction-to-board thermal resistance…
Part Number: SN65C1168E-SEP Hi,
Is TI willing to test the subject part in accordance with PEM-INST-001: Instructions for Plastic Encapsulated Microcircuit (PEM) Selection, Screening, and Qualification ? Please advise. Thank you.
Part Number: SN65C1168E-SEP Hi,
I'm using RS-422 transceiver part number SN65C1168E-SEP. Should the PCB trace impedance be 100-ohm or 120-ohm differential?
https://www.ti.com/product/SN65C1168E-SEP
Thanks,
Briana
Part Number: SN65C1168E-SEP Hi Team,
Can you help with this customer inquiry?
Will SN65C1168E-SEP be damaged if either an unpowered driver or receiver is driven from an externally powered device (say another driver/receiver on the bus)?
Section 6.5 of…
Part Number: SN65C1168E-SEP Hi,
For this IC, can customer applied input voltage when there is no Vcc?
For example, 5V at input of driver before voltage is applied to Vcc. If this possible, what is the maximum input voltage is allowed, it is the same as…
Part Number: SN65C1168E-SEP Hi there, maybe this is a very basic question. Can this device be used for RS-485? Any special considerations in designing as such?
Part Number: SN65C1168E-SEP I am interested to know the radiation tolerance of the SN65C1168E-SEP, RS-422 transceiver to Single Event Upset (SEU). Your radiation documentation for this part only lists the tolerance to Single Event Latchup (SEL). Our application…
Part Number: SN65C1168E-SEP Other Parts Discussed in Thread: DS34LV86T , DS34LV87T
Hi,
Can SN65C1168E-SEP operate at VCC=3.3V?
If yes, is there any Electrical Characteristics we can refer at this condition?
If no, can SN65C1168E-SEP at VCC=5V be connected…
Sorry for the delay. I learned that SN65C1168EMPWSEP is tested to a TI defined flow and qualification. See SN65C1168E-SEP Reliability Report
For more on Space-EP see
Space Enhanced Plastic gives designers a new solution for emerging low-Earth orbit commercial…
Part Number: SN65C1168E-SEP Greetings!
My customer has the following questions about the SN65C1168EMPWSEP:
If one of the drivers and/or receivers fails, is the other one isolated enough that it will still function?
Are there specific failure modes where…