Part Number: SN65C3223E Hi Experts,
We need your confirmation.
In the Datasheet, it is mentioned up to 1000 kbps it is supported and in the description, it is mentioned 100 kbps
kindly confirm the correct data rate. Thank…
Part Number: SN65C3223E Hello Team,
I observe a ripple voltage of 200mV at ~11kHz on pins V+ and V- at 3.3V Vcc and 4 x 100n caps; no load!
Shouldn't that be almost flat at no load or is that within the specification, please?
Thanks and Best Regards…
Part Number: SN65C3223E I’m working with the SN65C3223E in an application where we need to connect to a device via RS232. In this application, we do not need the automatic power down feature and have configured the circuit to disable the power down and…
Hi Cyril,
You could take a look at TRS3232E, which can operate from either 3.3 V or 5 V, supports baud rates up to 250 kbps, and has a high level of internal ESD protection which can be useful for external ports. If you wanted a transceiver with additional…