Other Parts Discussed in Thread: SN65CML100 Hi, does anyone know if I can use a SN65CML100 to convert LVPECL from a fiber receiver to 1.2 V CML for a Xilinx high speed serial transceiver. The interface has to be dc coupled so I need a level translator…
Hello Derek,
To be honest, the CDCLVP111-SP would be the most expansive part of our design. And to answer your question, I'm indeed looking for SEP parts.
I think I could go CML rather than LVPECL. Do you have something similar to the SN65CML100 that…
Part Number: SN65LVDT101 Other Parts Discussed in Thread: SN65CML100 ,
Hi,
I saw SN65LVDT101 is the only device that integrates 110-Ω Terminating Resistor. Can it be used as the LVPECL driver in below figure? Or, is there any other solution for LVPECL-to…
Thank you for the response.
I agree, DS15BA101 can driver 100 Ohm or 150 Ohm cables.
Just want to make sure there is no advantage to using the SN65CML100 device?
Both the DS15BA101 and the SN65CML100 look similar enough to me and it comes down to cost and…
Part Number: LMH0074 Other Parts Discussed in Thread: SN65CML100 , , DS15EA101 We are trying to interface the input of the LMH0074 to the output of the sn65cml100 driver. The output circuit is transformer coupled at the source driven into twisted shield…
Other Parts Discussed in Thread: TS3DV421 , TS3DV642 , SN65CML100 , TFP401 Hello,
I'm using a TS3DV421 as an HDMI multiplexer 2:1 and there is cross talk between channels.
When channel B is selected, the cross talk is acceptable and the receiver receives…
Other Parts Discussed in Thread: SN65CML100 , SN65LVCP1412 , DS15BA101 Hello,
I require a level translation for a 100 ohm 1GBPS LVDS serialized output (VOD=350mV) to a SFP module which requires a minimum VOD of 500mV. The SFP input is internally AC coupled…
Other Parts Discussed in Thread: SN65CML100 Hello,
The data sheet for the TSB81BA3D indicates a VOD output level for TPA and TPB of 265mV max into 56 ohms.
I actually measure a VOD on both TPA and TPB of about 740mV pk-pk when I have an active 1394B S800…
Other Parts Discussed in Thread: SN65CML100 , ADS6244 I want to interface the ADC ADS6244 with the DSPTMS320c6455 as I want high speed data capturing for me proto type test equipement. ADS6244 is a 14-bit ADC and having a Serial LDVS output. Can I directly…