Part Number: SN65DP149 Dear all,
Whether the SN65DP149 can be used for hdmi-to-hdmi design, which is equivalent to the use of an equalizer for HDMI.
I see that there are reserved HDMI interfaces in the sllu232 reference design, but there is no detailed…
Part Number: SN65DP149 Greetings!
I'm using the SN65DP149 as DP++ to DVI retimer, but right now I'm stuck with DDC problem. GPU is trying to reach the display through I2C, but on display's side is silence - constant 5V. Not even a single bit.…
Part Number: SN65DP149 Hi Team,
Please help to confirm the VSADJ resistor range.
Can we use 4.99K to GND on this pin? Because it is competitor-Parade(PS8407A) reference value, and we are trying to bom to bom replace it.
Thanks
Part Number: SN65DP149 Hi Sirs,
Sorry to bother you.
We would like to use DP149 to replace NXP PTN3360D
Besides the 40/48 pin different, have others Electrical characteristics or spec that we need carefully?
By the way, have dp149/ptn3306 spec compare form…
Part Number: SN65DP149 Other Parts Discussed in Thread: SN65DP159 1.Is SN65DP149/159 suitable for medical application(non-life threatening)
its an image processing applicaiton.
2.Are the drivers for windows 7 or windows compact embedded available to initialise…
Part Number: SN65DP149 Tool/software: Starterware Hi, Sir
I've got a basic question for SN65DP149 Chipset.
Is the chipset available on the DP 1.2-to-HDMI converting application? I'm not sure my choice of SN65DP149 for my target application is suitable…
Part Number: SN65DP149 Hi,
We are noticing that the signal coming out of the SN65DP149RSBT is adding significant jitter to the HDMI signal. Below is the input of the IC at pin 6 and 7 ( IN_D0x)
Below is the output of the IC on pin 24 and 25 (OUT_D0…
Part Number: SN65DP149 Hello,
I am working on a DP to DVI converter using SN65DP149 IC. Manufactured the PCB, assembled but it is not functioning.
I am using pin strapping for configuring the converter as follows:
I2C_EN/PIN is low, pin strap mode
EQ_SEL…