Part Number: SN65DP159 Other Parts Discussed in Thread: TDP1204 , TMDS1204 Hi team,
My customer asked for solution which can support HDMI2.1 specification.
I double checked SN65DP159 datasheet but it just supports HDMI2.0b only.
So could you comment right…
Part Number: SN65DP159 Other Parts Discussed in Thread: TMDS1204 , we new design HDMI 2.0 TX side used DP159 & TPD5S115YFFR solution.
Please help as follows:
1.please revuew circuit of attachment.
2.If the access circuit, we are worried that the DDC…
Part Number: SN65DP159 I am attempting to test a board that uses the SN65DP159 with an NVIDIA RT 1030 GPU. It is able to receive valid video during POST, so I am confident that the card is outputting a compatible format. However, when the driver loads…
Part Number: SN65DP159 Hi team,
Customer want a device that can support all HDMI output resolutions in the list. I'm not sure if SN65DP159 can work here. If not, could you pls help to pick out which resolution DP159 isn't able to support? And do…
Part Number: SN65DP159 Hi team,
Customer found an issue that after configure TMDS_CLOCK_RATIO_STATUS to 1, it will occasionally change to 0, which cause the HDMI can't output normally.
1) Does the configuration of TMDS_CLOCK_RATIO_STATUS affect the…
Part Number: SN65DP159 Hi team,
In datasheet spec, when SN65DP159 in retimer mode, duty cycle of out_clk is 40%-60%, but we test on EVM and the result is 37.5%. May I know the reason? Could you pls help to check it on EVM?
Thanks!
Rayna
Hi, David:
OK, later on I will try it as your said.
BTW, Si5324(clock chip) could be accessed through TCA9517A as below figure shown. So, I think the A side of TCA9517A should have no problem
Thanks in advance!
Best Regards!
Jason
Part Number: SN65DP159 Hi Team,
Customer is using SN65DP159 in their products, but failed in HDMI2.0 Intra-pair skew compliance test (HF1-4), customer's test result is 251mTbit, and limit is -150mTbit ~ 150mTbit. Can you help to check how we can to fine…