Part Number: SN65DP159 Hi team,
In datasheet spec, when SN65DP159 in retimer mode, duty cycle of out_clk is 40%-60%, but we test on EVM and the result is 37.5%. May I know the reason? Could you pls help to check it on EVM?
Thanks!
Rayna
Hi, David:
OK, later on I will try it as your said.
BTW, Si5324(clock chip) could be accessed through TCA9517A as below figure shown. So, I think the A side of TCA9517A should have no problem
Thanks in advance!
Best Regards!
Jason
Part Number: SN65DP159 Hi Team,
Customer is using SN65DP159 in their products, but failed in HDMI2.0 Intra-pair skew compliance test (HF1-4), customer's test result is 251mTbit, and limit is -150mTbit ~ 150mTbit. Can you help to check how we can to fine…
Part Number: SN65DP159 Hi Team,
My IPC direct customer iBASE is interested in SN65DP159RGZR for new project engagement, few questions from customer need your input:
Their application is for Display Port to HDMI Port, do SN65DP159RGZR is the most suitable…
Part Number: SN65DP159 Other Parts Discussed in Thread: TUSB1146 , TUSB1064 , DS160PR410 , TMDS181 , TDP1204 , TMDS1204 Hi
Could you help to suggest the following products
TYPE C Retimer - Support 10Gbps Retimer for USB 3.1 Gen2 and DP 1.4a
PCIE Retimer - PCIe…
Part Number: SN65DP159 Hi team,
Could you help confirm below questions?
1. VIL & VIH range for I2C_EN?
2. Recommended pullup & pulldown resistance for I2C_EN?
3. Reg 0Bh value will change automatically or need master's command for transition from…
Jason
Here is the resistor value,
[3-Level Input pins] Pull-up: 65k +/- 10% Pull-down: 0 to 65k + 10% [2-Level (LVCMOS) Input pins] Pull-up: 0 to 65k + 10% Pull-down: 0 to 65k + 10%
64.9k will work.
Thanks
David
Part Number: SN65DP159 Other Parts Discussed in Thread: TMDS181 Dear Sir,
Just like the tittle, does the DP159 work at the sink side? I want to use dp159 at source side and sink side, DP181 is more power consumption than DP159.
Best regards
David
Part Number: SN65DP159 Other Parts Discussed in Thread: SN75DP159 , 1. Does the SN65DP159 (or SN75DP159) support the p/n polarity reversal function whether it is a 40pin package or a 48pin package? Or is it only supported by 48pin models? 2. Does SN65DP159…
Part Number: SN65DP159 Other Parts Discussed in Thread: TDP0604 , TDP158 As the title states, does SN65DP159 support 1024x768 60Hz input? and if so, would the output still be 1024x768 60Hz or would this get scaled to 1080p60?
I understand it can automatically…