Cameron Wutzke said: Datasheet specifies a 2.175V maximum supply voltage, and long term exposure above that might cause permanent damage.
Hypothetically… do you know what would/could be damaged if the VCC was exposed to 3.3V for extended periods?
This…
Hey Shaswath,
Good to hear that you have the color bar working. Here is a snippet from the flickering video debugging guide that is relevant to where you are in testing.
Summary: When the color bar works and the DSI inputs don't, this means that there…
Part Number: SN65DSI84-Q1 Other Parts Discussed in Thread: DSI-TUNER Hi team,
I have a question here that if screen can't display the normal picture. What information can be read from the register of this IC using I2C for debugging?
BR,
Jimmy
Part Number: SN65DSI84-Q1 Hi team,
What is the behavior of the IRQ of SN65DSI84-Q? Please also answer the following questions: 1. When IRQ_EN = 1, what is the relationship between the status of the IRQ output and the 0xE5 register? 2. We saw the following…
Hi Vishesh,
Thanks for the update and detailed explanation.
Vishesh Pithadiya said: 1. [BIT:4] CHA_COR_ECC_ERR:
This bit is set when the SN65DSI84-Q1 detects a correctable ECC error. The SN65DSI84-Q1 does not have any error correction capabilities, so…
Part Number: SN65DSI84
Hi team
We have a device with a LVSD connector that will connect to three types of LCD panel.
- The First type of LCD panel can work with the frequency in range of 60MHz to 75MHz;
- The Second type of LCD panel can work with the…
Hey Nilesh,
Here is a reference Linux script that may help. Please have a look at the following thread.
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/549283/sn65dsi83-sn65dsi84-sn65dsi85---linux-driver/2006135#2006135
FYI as it…
Hey Liang,
As seen in the following chart the issues you seem to be having are due to CRC. ECC, and LLP errors.
This is most likely due to a line time issue/ setup issue, please have a look at the following guides:
Line time: https://e2e.ti.com/support…