Hi Ikram,
Thanks for your support.
Ikram Haque said: 3. We do not have a waveform from a setup to share here. In HS state, it would remain in HS mode similar to your waveform and it would not enter into LP state.
You can see my waveform that I…
Part Number: SN65DSI84-Q1 Hi team,
Please help clarify the following questions regarding the SN65DSI84-Q1 REFCLK:
1. What percentage of rise time and fall time are required?
2. What is the input capacitance of the SN65DSI84-Q1 REFCLK pin?
3. The…
Hi Park,
Park JungKyu said: Problem 1 : The LCD screen turns on normally, but then turns off and then turns on again when U12's 2Pin goes low.
The Pin 2 EN pin is used to enable/ disable the device. So this is expected that the device will reset/shutdown…
Part Number: SN65DSI84-Q1 Tool/software: Hi Team,
We need to drive LVDS display using DSI to LVDS (SN65DSI84TPAPRQ1 ) device for ASIL B cluster application.
Please let us know if considering ASIL b application. This IC is suitable. We are driving…
Part Number: SN65DSI84-Q1 Hello,
Hello,
I have identified part SN65DSI84-Q1 for my hardware architecture to provide DSI to LVDS functionality.
I want to make sure that this part can correctly drive my TFT module, particularly with regard…
Part Number: SN65DSI84-Q1 Other Parts Discussed in Thread: SN65DSI84 Tool/software: Hi, TI expert
A customer has a question regarding the SN65DSI84-Q1 output.
- Application : Video splitter and channel display device
The current hardware configuration…
Part Number: SN65DSI84-Q1 Other Parts Discussed in Thread: SN65DSI83 Hi team,
My customer wants to use this device to transmit DSI data. However, their DSI rate is 2Gbps/lane.
Can our device support this? Is there any other device that can convert…
Part Number: SN65DSI84-Q1 Other Parts Discussed in Thread: SN65DSI84 , SN65DSI83 Tool/software: We are using the SN65DSI840Q1 chip as a bridge from MIPI to LVDS. The MIPI signal comes from the Orange Pi CM4, and the LVDS output is connected to the LCD…
Part Number: SN65DSI84-Q1
Tool/software:
Hi BU team
How my customers understand the Vpsn in below table for SN65DSI84-Q1? I think that it means ripple voltage requirement, is it right? Vipple voltage is measured via scope with 20MHz bandwidth limit…