Part Number: SN65HVD01 Hi,
Is it possible to finalize Test orders manually or do they need to complete the document flow ?
Could you send us an example of a delivery note between TEXAS -IKOR ?
Part Number: SN65HVD01 I measured A with an oscilloscope.
Setting
* VCC, VL = 3.3V
* nRE / DE = Pull up (3.3v / 6k Ohm)
* Terminator Resistor = Side 120 Ohm
Ch 1 = SN65HVD01 R Digital Output (2pin)
Ch 2 = SN65HVD01 A Bus I/O
The…
Part Number: SN65HVD01 Other Parts Discussed in Thread: THVD1500 , THVD1410 Hi Sir
May SN65HVD01 can take signal from RJ45 and the get Differential signal transfer to Single-Ended?
or there have other suggestion part?
Bogey
Part Number: SN65HVD01 Hi dear supporting team,
customer is using SN65HVD01, want to need double check with you:tks!
the Vl=1.8V, VCC=3.3V, when Vl=1.8V shows up, but Vcc 3.3v is not supplied, i.e. Vcc=0V, will it cause damage?
Part Number: SN65HVD01 I want to know the communication distance according to the voltage supplied to the Transceiver.
- Is there a difference in communication distance between 3.3v and 5v?
- What is the maximum communication distance when the supply…
Part Number: SN65HVD01 Other Parts Discussed in Thread: SN65HVD10 Hello,
I am having a new question about the SN65HVD01 transceiver :
Considering 2 transceivers very close together, in the same environment (identical temperature and power supply)…
Part Number: SN65HVD01 Spec
: SN65HVD01 (power Supply 3.3v)
: Cable awg 24 (twist + shield)
: data rate 200kbps under
: Stub line 1 (1:1 communication)
1) What is the maximum cable length that can be RS 485 communicated in the above situation…
Hi Tom,
I'm not very familiar with the HDLC protocol. From what I understand, it is a data-layer protocol used for point to multi-point asynchronous systems. As RS-485 is a physical-layer protocol that also fits this description, I believe the two would…
Part Number: SN65HVD01 Other Parts Discussed in Thread: THVD1450 Hi,
Do we have upgraded part of SN65HVD01 supporting both 3.3V and 5V RS-485 to replace XR33202? Thanks.
Best Regards.
Chen
Part Number: SN65HVD01 Other Parts Discussed in Thread: TLV3201 , Does the schmitt trigger on the A and B inputs shown in the receive equivalent circuitry trigger at 0.7VL for High Logic levels and 0.3VL for Low Logic Levels?