Part Number: SN65HVD01
Hi,
When we test the IBIS model, we find accuracy problem in it, anyone could update it?
ryt1097699_2
REB_P3v3:
AB_hs:
The attachment is as below:
sllm229c.zip
Other Parts Discussed in Thread: SN65HVD01 Hi team,
For RS485 traces on SN65HVD01 A/B pin.
1. Does these two traces "differential" in layout design?
2. Does these two traces require impedance control in layout design? If yes, what is the impedance…
Other Parts Discussed in Thread: SN65HVD01 Dear Team,
Just to verify one little thing wasn't mentioned on the datasheet.
Should the SN65HVD01 EP pad be connected to GND ?
Best Regards,
Nir.
Other Parts Discussed in Thread: SN65HVD01 Questions about the SN65HVD01 part: 1. Can it be used as a standard RS-422 transceiver? 2. Do you have a full-duplex version of it? 3. If ans of #2 is no, do you recommend someone to use two SN65HVD01 parts to form…
Other Parts Discussed in Thread: SN65HVD01 Hi,
Please let me know whether the following points for SN65HVD01 IBIS model are correct.
Regarding the definition of [Ramp], AB_hs's [Ramp] are smaller than AB_ls's. Is this correct ?
※AB_hs high speed AB…
Part Number: THVD1451 Other Parts Discussed in Thread: SN65HVD01 Hello,
Does TI have any full duplex RS485 transceivers that can operate at 1.8V?
Thanks, Adam
Minqi,
Do you have more information about the system level requirement on this spec? For now I would recommend SN65HVD10 or SN65HVD01 for comparison.
device
SN65HVD10
SN65HVD01
tPLH
5ns 8.5ns 16ns
6ns 15ns 25ns
tPHL
5ns 8.5ns 16ns
6ns 15ns 25ns
…
Hello Shinu,
Please take a look at the SN65HVD01 device. It is a 3.3-V-powered RS-485 transceiver that supports a separate 1.8-V logic rail.
Regards, Max