Part Number: SN65HVD12 Other Parts Discussed in Thread: TCAN1043 https://www.nxp.com/docs/en/data-sheet/TJA1041A.pdf
Would you advice a suitable solution to replace?
Hi Sagar,
Please see reply on post here: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1311754/sn65hvd12-more-than-5-devices-on-the-bus-fails
We can continue discussion on this topic on that thread so we don't have two open with…
Other Parts Discussed in Thread: SN65HVD12 , SN65HVD72 Hello,
currently I use a SN65HVD12 to make a RS485-communication happen. This works quite well.
But I think that in some circumstances the "network" does some unhealthy stuff to my PCB.
-->…
Other Parts Discussed in Thread: SN65HVD12 , SN75HVD12 Dear Sirs
I have some issue about the max LENGTH of SN65HVD12
The following link is The RS-485 Design Guide.
From the equation: Lstub<= tr/10*v*c and datasheet of SN75HVD12
The max tr is 300ns.
So…
Hello I have a question regarding SN65HVD12, In page 14 the following image is shown, as equivalent input circuits. If A and B are protected with 16 volt Zeners, with regards to compliance in energy limited circuits, can these be listed as protection…
Other Parts Discussed in Thread: SN65HVD12 , SN65HVD72 , SN65HVD75 Hello, all
Now we are considering to use SN65HVD12.
I would like to know its FailSafe functionality, with including basic standard for RS485 itself.
Please see the comment below and feedback…
Unfortunately, we do not have a 3.3 quad line driver with enough absolute max headroom for TVS diode for lightning suppression.
I did search through our other EP interface offerings. We do not have any 3.3V quad RS485 transceivers. We do have one…
Dear Bart,
Thanks for your kindly help. I think SN65HVD12 is a good choice.
If SN65HVD12 used, whether the clamp voltage with BAT54S should be 3.3V or still 5V?
Best Regards
Andy
hi rahul..
i m thinking to use sn65hvd12 rs485 transciever interface with msp430g2553 with same schematic as you and pallav used.
Actually in our application we want that controller shoul read data from fuel sensor that gives rs485 output.
While msp…