Part Number: SN65HVD71 Other Parts Discussed in Thread: SN65HVD1471 , SN65HVD1470 , SN65HVD70 , , SN65HVD73 , SN65HVD1473 , SN65HVD74 , SN65HVD1474 , SN65HVD1476 , SN65HVD76 , SN65HVD77 , SN65HVD1477 I can see that the ESD levels are higher and the thermal resistance…
Part Number: SN65HVD1471 Other Parts Discussed in Thread: SN65HVD1474 Hi experts
I would like to know if this device can be used for signaling above 400kbps, for example at 950 or 1000 kbps.
I have an application that I am already using it at a higher…
Part Number: SN65HVD1471 Hi, I met a problem when i tried to interface my SN65HVD1471 transceiver with MAX14850 isolator. Please refer to my connection below,
R(Transceiver) - INA1- OUTB1 - Rx(MCU)
Tx(MCU) - INB1 - OUTA1 - D(Transceiver)
Transceiver…
Part Number: SN65HVD1471 Hi,
SN65HVD1471 transceiver IC produces irrelevant output. To check hardware i just shorted Tx and Rx pins of IC and connected the differential pair by connecting 120 ohms across A,B and Y,Z, and given 3.3V to vcc pin and connected…
Part Number: SN65HVD1471 Hi,all
The SN65HVD1471 device can be used for RS-422 interface? I cann't find the datasheet said it can support RS-422 interface.
Is there any reference design for RS-422?
Part Number: SN65HVD1471
Hi...
At the differential pair of SN65HVD1471 i.e. A,B,Y,Z pins is there any need to connect some resistors? If yes could you please mention the specification.
And R pin of transceiver is denoted as digital output in datasheet…
Part Number: SN65HVD1471 Dear sir,
i bought SN65HVD1471, for communicating PIC18F65K40 using RS422 protocol. I can't able to understand, how it's interfacing with DB9 connector and also where to drive output and to give input in this transceiver IC.…
Rajesh,
You can consider SN65HVD1471, which has better ESD protection but might not be enough for the surge current. What's your schedule of product release? We're developing some RS485 transceivers with surge protection feature. You could evaluate them…
This spreadsheet tool makes it easy to look up what the recommended pin to pin capable RS-485 transceivers to replace old TI RS-485 transceivers.
/cfs-file/__key/communityserver-discussions-components-files/138/1777.Recommended-New-RS_2D00_485-parts-for…