Part Number: SN65HVD1792-EP The operating air temp. of this device is restricted to +105deg.C.
But I don't understand the reason from the following.
(1) The device is "Enhanced Products", having the caracteristic of extended temp., -55deg.C to +125deg…
Part Number: SN65HVD1792 Hi,
Good Day. What is the input impedance of each receiver input of SN65HVD1792? Thank you very much.
Best Regards,
Ray Vincent
Part Number: SN65HVD1792 At the top of the datasheet it shows that SN65HVD1792...
• Bus-Pin Fault Protection to: – > ±70 V ('HVD1785, 86, 91, 92)
However later in the datasheet it shows under absolute maximums...
'HVD1785, 86, 91, 92, 93 A, B pins…
Part Number: ISO1432 Other Parts Discussed in Thread: SN65HVD33 , SN65HVD1792 , THVD1452 Hello
Now I am designing RS-485 interface circuit using ISO1432.
The following transceiver ICs will be used for the components to be communicated with.
- Transceiver…
Part Number: SN65HVD1792 Other Parts Discussed in Thread: MAX232 On a card I am working on there are two rs-232 to rs-485 circuits, one contains one ISL849IB and is connected to a max232. The second circuit again has a max232 but then has two ISL849IBs…
Part Number: SN65HVD1792-EP I'm evaluating two transceivers with fault protection (Linear's LTC2865 and SN65HVD1792-EP).
During +ve voltage fault and higher than Vcc common mode voltage conditions, LTC part says that some current may flow back to supply…
Part Number: SN65HVD1792-EP How is it possible to obtain the SN65HVD1792-EP safety and reliability information? MTBF (Mean timen between failures) and FIT (Failures in Time. Failures per 1e9 working hours)?
Thanks in advance
Part Number: SN65HVD1792 Hi there,
My customer supplies 5V to the Vcc of HVD1792 but would like to know if the I/O pins can work at 3.3V voltage level.
From the datasheet, the min. of VIH is 2V so I guess it might work at 3.3V?
Best regards, …