Part Number: SN65HVD232Q-Q1 Hello,
The customer uses the SN65HVD232Q-Q1 product without an external 120 ohm resistor, and the hidden voltage level of CAN-H and CAN-L is only 1.3V, which is much lower than the 2.3V in the manual. The impedance test is…
Part Number: SN65HVD232Q Tool/software: Hi Team,
Request you to share the reflow graph and reflow conditions for the part number SN65HVD232QDRQ1
Regards,
M.Sandhiya Subashree
Part Number: SN65HVD232Q-Q1
Tool/software:
Hi Experts,
Good day!
I'm looking for the thermal resistance information for the p/n below. No information in the datasheet can you share with us the thermal resistance and theta-JC of the device?
…
Part Number: SN65HVD232Q Hi Team
My customer needs to learn if SN65HVD232Q is CUPstructure (referring to active circuitry on the die underneath the bond pads) to recognize the material, could you kindly provide the information?
Regards,
Part Number: SN65HVD232Q Hello,
These parts did not come with an ESD bag, they only came in ESD tubes. Please let me know if this is normal for this package and MSL type.
Parts came from AVNET.
Please let me know if you need additional information…
Part Number: SN65HVD232Q Can we use TCAN332DCNR as an alternate for SN65HVD232QDR. If possible Please suggest an alternate for SN65HVD232QDR with same pinout and functionality as we don't have SN65HVD232QDR in stocks.
Thanks in advance.
Part Number: SN65HVD232Q Other Parts Discussed in Thread: TCAN334 , TCAN332 , SN65HVD232 , TCAN330 , TCAN337 Can you please confirm SN65HVD232QDRQ1 will be used as an alternate for SN65HVD232QDR. We need same pinout and functionality. Is there any major…
Part Number: SN65HVD232Q-Q1 Hello,
We would like to do Bulk current injection test on the CAN communication line.
Before going in to the actual lab test we would like to simulate the bulk current injection in the CAN communication line.
We know…
Part Number: SN65HVD232Q-Q1 I need to use this SN65HVD232Q-Q1 IC for CAN interface and was unable to get the req result. My design gives a noisy waveform of CANH and CANL. The voltages I get are" 1: 3.3V, 2: 0V, 3: 3.3V, 4: 3.3V, 5: 0V, 6: 2.25V, 7: 2…
Hi,
I have a question about definition of Vod in datasheet.
There are two descriptions of the VOD(D) upper of the data sheet on page 7.
What difference is the upper and lower ?
Although it has been terminated with 60Ω, the minimum value of…