Part Number: SN65HVD234-Q1
Dear all,
I need to connect 2 devices with canbus interface.
I have no ground reference. There are available only the CanH, CanL and Power+ pins.
How can I connect them in order to exchange can messages?
The positive pin of…
Part Number: SN65HVD234 Dear TI Team,
my customer would like to use SN65HVD234D in a medical application and would need some information about the Environmental Air Pressure and Elevation the device can be used.
Can you please provide us this informat…
Part Number: SN65HVD234 Hello,
We are using the CAN transceiver for our projects.
From the datasheet of SN65HVD234, I can see that the IC is ISO 11898-2 and GIFT/ICT compliant.
Could you please share the below reports:
- ISO 11898-2 compliancy proof
- …
Part Number: SN65HVD234 Hi TI team .
My customer used SN65HVD234 in their OBD product and needs the value of SN65HVD234 which should reply to upstream customer.They have removed the chip from PCB and allow the test condition(like the red block in the…
Part Number: SN65HVD234 Hi TI team .
My customer used SN65HVD234 in their OBD product and needs the value of SN65HVD234 which should reply to upstream customer.They have removed the chip from PCB and allow the test condition(like the red block in the…
Part Number: SN65HVD234 Hi
I want to have CAN network of 64 nodes with minimum possible overall current consumption using SN65HVD234.
The idea is to keep all devices in standby and enable one driver only. My problem is how to enable driver.
Bus speed…
Part Number: SN65HVD234 Dear Sir,
My customer have a design for SN65HVD234 and CAN330, they found that both product CANH and CANL differential output actual peak to peak voltage is 1.96V, it cannot meet ISO11898 standard, and if cannot meet datasheet…
Part Number: SN65HVD234 Other Parts Discussed in Thread: TCAN334 , Hi Michael,
Having read the post and datasheet for the CAN Transceiver SN65HVD234DR, operating @3.3V, my question - Does this device has dominant time-out (DTO) protection on the output lines…
Part Number: SN65HVD234
Hi,
I am currently designing something with this CAN BUS transceiver. And I saw someone post this circuit diagram before, may I kindly ask few questions regarding to this circuit?
1. Is it a must to have R20 & R21
2. What…
Part Number: SN65HVD234 Is there a minimum termination resistance value (across CANH and CANL) to guarantee that the R output will correctly duplicate the data sent on the D input? We have a problem with our power control software, which depends on the…