Part Number: SN65HVD234 Our product is designed with a SN65HVD234DR CAN transceiver. We have found on multiple occasions recently that when doing continuity tests on the harness the product is built into that the CAN Low line has a small resistance to…
Part Number: SN65HVD234 Hi,
Could you please confirm that the SN65HVD234 part will operate correctly against the ISO11898-2 specification section 5.4 with a maximum dominant state differential input voltage of 8V.
Many thanks,
Dan
Part Number: SN65HVD234 1. There is no figure given in the datasheet for receiver input resistor matching.
2. There is no figure given in the datasheet for Driver symmetry.
Can those values be provided?
Part Number: SN65HVD234 Other Parts Discussed in Thread: TCAN334 Hi Team,
My customer is using the SN65HVD234 on a 3.3V-only application and running into EMI issues due to the high common-mode voltage. They would like to know if they can re-bias to a lower…
Other Parts Discussed in Thread: SN65HVD234 , TCAN332 Hi teams,
I have a question about SN65HVD234.
Please let me know about the follows.
The device is driving in "1" state.
I think it is in Hi-impedance, so it has driven somewhat.
In TCAN332…
Part Number: SN65HVD234 Dear team,
our customer is facing a temperature issue with the SN65HVD234 at could temp. Attached please find an explanation as a starting point. I also received measurements that I can send offline. Here is the description of the…
Hi Billy,
Just checking back in. Have you received new test boards to continue the testing? If so, have you seen the same issue or has it resolved itself?
Regards,
Max
Part Number: SN65HVD234 Other Parts Discussed in Thread: TCAN334
Dear Team,
our customer has problems passing the EN55014 spec / ‘Conducted disturbance additional terminals’.
The HVD234 is above the peak spec for lower frequencies (< 1MHz).…
Part Number: SN65HVD234-Q1 Hi Ti Team:
I used SN65HVD234-Q1 for can bus communication .
But I found my recessive voltage have a slope rate , it's not shown as our datasheet ,a parrel line with X axis.
The picture shown as below .
Please help to advise…