Part Number: SN65HVD234 Hi,
I have designed a product using CAN Transceiver SN65HVD234QDRQ1, So please review the attached design to avoid any design related issues.
Part Number: SN65HVD234-Q1 Thanks in advance for any help.
I just created a new design using the 3.3v transceiver coupled with an MCP2515.
Everything works fine with the MCP2551 (at 5 volts) with the MCP2515 at 3.3v on the bench.
My new design doesn…
Part Number: SN65HVD234 Other Parts Discussed in Thread: TCAN1042-Q1 , TCAN1051-Q1 , TCAN330G , TCAN332G I read the TI app note SLLA279A on minimum distance between CAN nodes. The solution offered was to increase the length of the cable joining the CAN nodes…
Part Number: SN65HVD234 Hi,
the max. output current of my DC/DC is only 60mA. I would like to know if this power supply is sufficient.
In the datasheet Icc is specified without load an so not helpful. The max. diferential output voltage is 3V. Hence the…
Hi Henry,
ISO 11898-2 was developed for 5V automotive systems and does not include any 3.3V requirements. When we say "compatible with ISO 11898-2" we are saying that the 3.3V part(s) are designed to meet as many of the ISO specs as possible but there…
Other Parts Discussed in Thread: SN65HVD234 Hi team,
My customer is using the SN65HVD234 now and meet the broken problems. When solder off the chip, and test the resistance of the chip. The Vcc to ground resistance isn't infinite large and only 60kohm…
Part Number: SN65HVD234 Hi Team, I believe it is no ploblem if applying 3.3V to D (1pin) and Rs (8pin) under no VCC because of ABS Max ratings in datasheet. Is my understanding correct? Best Regards, Yaita / Japan disty
Hi Yaita-san,
When the driver is in the off state (TXD high = recessive level) the bus pins are high impedance but if the driver was stuck in the on state (TXD low = dominant) the FET will be on and the possibility for damage is there if bus fault protection…
Part Number: SN65HVD234 I am having issues with the CAN transceiver in the title. I have attached a screenshot of the input to the D line and the output of the CAN_L line. We have checked that the chip is soldered the right way and that the EN, Vcc are…
Other Parts Discussed in Thread: SN65HVD234 I'm working on a product that uses SN65HVD234 for the CAN bus, but a number of devices in the current lot have very large numbers of CAN errors. We've had quite a few lots where we didn't notice this happening…