Part Number: SN65HVD3083E Hi
I'm considering power source for SN65HVD3083E.
As the power dissipation of IC itself, we can refer 136mW as maximum from datasheet.
So, if VCC is 5V, the current of IC would be calculated as 136mW/5V = 27.2mA as…
Part Number: SN65HVD3083E Hi
The short circuit output current is 250mA and it is defined in TIA/EIA-485A Standard.
Does it mean there is possibility of 250mA current flowing when driver's output are shorted each other (in other words, Vod = 0V)…
Part Number: SN65HVD3083E Other Parts Discussed in Thread: THVD1550 , Hi
We want to estimate total current consumption in two case.
1. Normal operation (VCC=5V, 1Mbps)
2. Output short
>1.Normal operation
The device has driver and receiver…
Part Number: SN65HVD3083E Hi,
I made a board with the device of SN65HVD3083E and evaluated it. However, due to the influence of noise on the signal line, I am considering adding the following contents to the circuit. · Pull up A signal to 5 V with 10kΩ…
Part Number: SN65HVD3083E Hi,
I am doing a noise test on a device using SN65HVD3083E device. I attach a circuit diagram. Since there is only one communication partner, it performs one-to-one communication. For noise, noise superimposed from the AC 100…
Part Number: SN65HVD3083E Hi,
I am doing a noise test on a device using SN65HVD3083E device. I attach a circuit diagram. Since there is only one communication partner, it performs one-to-one communication. For noise, noise superimposed from the AC 100…
Other Parts Discussed in Thread: SN65HVD3083E Hi
We want to confirm the input specification for driver.
The following figure is on the datasheet (Figure 4)
According to this figure, the input is given with 500KHz, 50% duty, tr <6ns, tf <6ns…
Part Number: SN65HVD3083E Hello Adrian, Thank you for your reply. And I'm sorry for my late reply.
If possible, please let me know the device name and the test result of DE pin. (If the test result can be applied to SN65HVD3083E.)
If the test result…
Part Number: SN65HVD3083E Hi,
I previously asked questions about SN65HVD3083 E in the following thread. I got an answer of the following contents to be informed. Among them, there is u.l. = 5.6. How do you calculate this "5.6"? Can you teach me the…